SBAS945B February 2022 – December 2024 AMC23C14
PRODUCTION DATA
The AMC23C14 is operational when the power supplies VDD1 and VDD2 are applied, as specified in the Recommended Operating Conditions table.
The four comparators on the high-side (Cmp0 to Cmp3) function as two independent window comparators when the voltage on the REF pin is below the VMSEL threshold. If the voltage on the REF pin exceeds the VMSEL threshold, the negative comparators (Cmp1 and Cmp3) are disabled, and Cmp0 and Cmp2 function as two independent positive comparators, as described in the Reference Input section.