SBASAZ3 October 2025 AMC0206M25-Q1 , AMC0306M25-Q1
PRODMIX
If a full-scale input signal is applied to the AMC0x06M25-Q1, the device generates a single one or zero every 128 bits at DOUT. Figure 7-6 shows a timing diagram of this process. A single 1 or 0 is generated depending on the actual polarity of the signal being sensed. A full-scale signal is defined as |VINP – VINN| ≥ |VClipping|. In this way, differentiating between a missing AVDD and a full-scale input signal is possible on the system level. See the Diagnosing Delta-Sigma Modulator Bitstream Using C2000™ Configurable Logic Block (CLB) application note for code examples of diagnosing the digital bitstream.