SBAU479 December 2024 TAA3020
Open the PPC3 application in the directory chosen for the GUI installation in Section 5.1. Figure 5-2 shows the resulting app center window. Click on the TAA3020 app title.
Figure 5-2 PurePath Console 3 App CenterThe TAA3020 GUI is designed to work with up to four devices at any time. As shown in Figure 5-3, choose the 1 device radial button and click New.
Figure 5-3 Initial GUI ConfigurationAs shown in Figure 5-4, the GUI opens to the Audio Config tab.
Figure 5-4 Audio Config TabBefore changing any parameters, check the lower left corner of the PPC3 window, as shown in Figure 5-5, to verify that the EVM is connected. If no EVM is detected, the text will read TAA3020 offline. If the EVM is detected, a Connect button appears. Clicking this button connects the hardware.
Figure 5-5 Hardware ConnectWhen the hardware is connected, the Connect button changes to read Disconnect, and the device is ready to be configured.