SBOA586A February   2024  – May 2025 OPA182 , OPA186 , OPA187 , OPA188 , OPA189 , OPA333 , OPA387 , OPA388

 

  1.   1
  2.   Abstract
  3. Benefit of Zero-Drift Amplifiers
  4. Internal Operation of Choppers
  5. Chopping Input Current Transients
  6. Bias Current Translation Into Offset
  7. Chopping Current Transient Impact on Offset Voltage
  8. Input Bias Current versus Bias Transients
  9. Amplifier Intrinsic Noise
  10. Chopper Transient Noise
  11. Procedure for Selecting a Zero-Drift Amplifier
  12. 10Summary
  13. 11References
  14. 12Revision History

Chopping Current Transient Impact on Offset Voltage

Figure 3-5 illustrates the amplifier transient input current due to the charge injection and clock feedthrough of the chopper input metal–oxide–semiconductor (MOS) switches. When these input transient currents flow through the feedback network and source impedance connected to the amplifier, the transients convert into voltage. The transients are very fast compared to the bandwidth of the op amp, so the transients do not fully settle. The average of the AC voltage signal from the chopping transients has a non-zero value. This average value acts as an additional input offset voltage that adds to the offset of the amplifier. Depending on the magnitude of the source and feedback impedance, the offset due to the chopping transients can be either negligible or can be significant compared to the offset of the amplifier. The specific resistance value where the transients begin to be significant depends on the bandwidth of the amplifier, chopping frequency, and transient IB glitch magnitude.

Figure 5-1 shows a simple TINA-TI model for OPA188 that includes the transient current pulses (IG1 and IG2), bandwidth, and input capacitance. The current transient on the non-inverting input flows through the source impedance, and the transient on the inverting input flows through the impedance network. If these two transients are identical, and the feedback impedance matches the source impedance, then the transient input currents create offset voltages from the feedback and source impedance that cancel each other.

OPA189, OPA388, OPA333, OPA187,OPA188, OPA186, OPA182, OPA387 TINA-TI model for Chopper
                    Transients on OPA188 Figure 5-1 TINA-TI model for Chopper Transients on OPA188

Figure 5-2 shows the response for the circuit shown in Figure 5-1. Since there is a slight mismatch in the current transients, the transients do not fully cancel and the output shows an offset error signal that varies with time. The DC average of the output offset signal is 25.8µV. Figure 5-3 shows the response for the same circuit with the feedback resistor shorted. Since RFB is shorted, there is no canceling effect between the inverting and non-inverting signal. Thus, the average output offset increases to 204µV. Figure 5-4 shows the response for the same circuit with the source resistor shorted. Again, there is no canceling effect between RFB and Rs since Rs is shorted (average offset is –187µV).

OPA189, OPA388, OPA333, OPA187,OPA188, OPA186, OPA182, OPA387 Simulated Output Offset for
                    OPA188 Model (RFB = Rs = 100kΩ) Figure 5-2 Simulated Output Offset for OPA188 Model (RFB = Rs = 100kΩ)
OPA189, OPA388, OPA333, OPA187,OPA188, OPA186, OPA182, OPA387 Simulated Output Offset for
                    OPA188 Model (RFB = 0Ω, Rs = 100kΩ) Figure 5-3 Simulated Output Offset for OPA188 Model (RFB = 0Ω, Rs = 100kΩ)
OPA189, OPA388, OPA333, OPA187,OPA188, OPA186, OPA182, OPA387 Simulated Output Offset for
                    OPA188 Model (RFB = 100kΩ, Rs = 0Ω) Figure 5-4 Simulated Output Offset for OPA188 Model (RFB = 100kΩ, Rs = 0Ω)

It is undesirable for the bias current transients of a chopper amplifier to produce offsets that are larger than the Vos of the device. The offset voltage generated by these current transients is dependent on the magnitude of the source impedance and the impedance of the feedback network. Figure 5-5 shows a graph of OPA388 offset voltage versus source impedance. The flat region on the left-hand side of the graph is where the inherent offset of the amplifier is dominant. The region where the curve increases with source impedance is where the current transients dominate the offset. In general, do not use the chopper amplifier with the larger source impedances where the transients dominate. The transition point where the source impedance is considered large is different for each chopper amplifier. Table 5-1 provides a list of chopper amplifiers and the associated maximum impedance to avoid the increase in offset voltage.

OPA189, OPA388, OPA333, OPA187,OPA188, OPA186, OPA182, OPA387 Offset vs Source Resistance
                    for OPA388 Figure 5-5 Offset vs Source Resistance for OPA388
Table 5-1 Maximum Recommended Rs and Feedback Resistance (Rf || Rg)
Op Amp Model Maximum Recommended
Rs and Rf||Rg (kΩ)
OPA189 1
OPA388 10
OPA333 1000
OPA187 500
OPA188 10
OPA186 500
OPA182 10
OPA387 10