SBOA590 November   2024 OPA186 , OPA206 , OPA210 , OPA2210 , OPA328 , OPA391 , OPA928

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Input Offset Voltage (VOS) Definition
    1. 1.1 Input Offset Voltage Drift (dVOS/dT) Definition
    2. 1.2 VOS and VOS Temperature Drift Inside the Amplifier
    3. 1.3 Laser Trim to Adjust Performance
    4. 1.4 Package Trim (e-Trim™) to Adjust Performance
  5. 2Input bias current (IB) definition
    1. 2.1 Input Bias Current (IB) and IB Temperature Drift Inside the Amplifier
    2. 2.2 Derivation of IB Conversion to VOS
    3. 2.3 Internal Bias Current Cancelation
    4. 2.4 Super Beta Input Transistors
  6. 3Other Factors Influencing Offset
    1. 3.1 Finite Open Loop Gain (AOL)
    2. 3.2 Common Mode Rejection Ratio (CMRR)
    3. 3.3 Power Supply Rejection Ratio (PSRR)
    4. 3.4 AOL, CMRR, and PSRR Over Frequency
    5. 3.5 Electromagnetic Interference Ratio (EMIRR)
    6. 3.6 Mechanical Stress Induced Offset Shift
    7. 3.7 Parasitic Thermocouples
    8. 3.8 Flux Residue and Cleanliness
  7. 4Zero-drift Amplifiers to Minimize VOS and VOS Drift
  8. 5Calibration of VOS, IB, and Gain Error
  9. 6References
  10. 7Revision History

Internal Bias Current Cancelation

The op amp input pins are connected to the base of the transistors in the differential input pair. The bipolar transistors are current controlled devices, so base current is required to properly bias the input stage (see Section 2.1). The choice of input stage collector current biasing depends on the bandwidth, noise, and slew-rate requirement for the op amp. The base current of the input transistors will be the collector current divided by the current gain of the transistor (β). Thus, the input bias current, IB, for bipolar devices will depend on the specific product requirements and process technology. Nevertheless, a typical range of uncorrected input bias currents is in hundreds of nano-amps to micro-amps. For some applications, the uncorrected bias current value would introduce large errors that would be considered unacceptable. To solve this issue, the integrated circuit design method bias current cancellation is used to significantly reduce bias current.

The input bias current cancellation is a method where the transistor base current is monitored and an equal but opposite current is summed into the op amp input terminal to cancel the base current (see Figure 2-12). If the cancellation circuit worked perfectly, the input bias current seen from outside of op amp would reduce to zero. However, there is a tolerance in the canceling current so that some residual bias current remains. Typically, the improvement due to input bias current cancellation reduces IB by a factor of 100. Figure 2-12 shows the bias current reduced from 10 nA to about 1 nA. Also, without bias current cancellation the bias current of bipolar devices always flows in the same direction. For an NPN device, base current flows into the base, and for PNP it flows out of the base. However, when bias current cancellation is used, the residual current after the correction can flow in either direction.

Using bias current cancellation also has an impact on input bias current offset (IOS). In general, for devices that do not use bias current cancellation the IB tends to be much larger than IOS (approximately 10x). This is because the input transistors are well matched. Conversely, when bias current cancellation is used the residual IB left after the cancellation is an error term, and the two inputs is no longer well matched. Thus, for devices that use bias current cancellation IB is approximately the same magnitude as IOS. When IB >> IOS, the impact of IB can be reduced by matching the impedance of the feedback network and non=inverting input of the op amp. Conversely, when IB ≌ IOS, matching the impedances no longer helps reduce the effects of IB and may in fact double the error.

Table 2-2, and Table 2-3 compare a device without IB cancellation to one with IB cancellation. Most important notice that the absolute magnitude of IB is much lower when IB cancellation is used (-35 nA vs ±4.5 nA). Also, notice that without IB cancellation IB >> IOS, but with cancellation IB ≈ IOS. Finally, notice that without IB cancellation, the polarity of IB is in one direction, whereas it is in both directions with IB cancellation (-35 nA vs ±4.5 nA). The negative polarity for IB without IB cancellation indicates an PNP input structure.

OPA206 Internal Bias Current
                    Cancellation Figure 2-12 Internal Bias Current Cancellation
Table 2-2 IB and IOS for Device Without Bias Current Cancellation (LM358B)

PARAMETER

TEST CONDITIONS

MIN

TYP

MAX

UNIT

LM358B | INPUT BIAS CURRENT

IB

Input bias current

-10

-35

nA

TA = -40°C to 85°C

-60

IOS

Input offset current

±0.5

±4

nA

TA = -40°C to 85°C

±5

Table 2-3 IB and IOS for Device with Bias Current Cancellation (OPA209)

PARAMETER

TEST CONDITIONS

MIN

TYP

MAX

UNIT

OPAx209 | INPUT BIAS CURRENT

IB

Input bias current

VCM = 0 V

TA = 25°C

±1

±4.5

nA

TA = -40°C to 125°C

±15

IOS

Input offset current

VCM = 0 V

TA = 25°C

±0.7

±4.5

nA

TA = -40°C to 125°C

±15