SBOS061C February 1997 – October 2024 XTR105
PRODUCTION DATA
Remote connections to current transmitters are sometimes subjected to voltage surges. Limit the maximum surge voltage applied to the XTR105 to the lowest practical value. Various zener diodes and surge clamping diodes are specially designed for this purpose. Select a clamp diode with as low a voltage rating as possible for best protection. For example, a 36V protection diode allows proper transmitter operation at normal loop voltages, yet provides an appropriate level of protection against voltage surges. The XTR105 is specified to an absolute maximum loop voltage of 40V.
Most surge protection zener diodes have a diode characteristic in the forward direction that conducts excessive current, possibly damaging receiving-side circuitry, if the loop connections are reversed. If a surge protection diode is used, use a series diode or diode bridge for protection against reversed connections.