SBOS844D May 2021 – August 2025 INA234
PRODUCTION DATA
For the INA234 to report current values in Amperes, a constant conversion value must be written in the calibration register that is dependent on the selected CURRENT_LSB and the shunt resistance used in the application. The value of the calibration register is calculated based on Equation 1. The term CURRENT_LSB is the chosen LSB step size for the CURRENT register where the current is stored. Equation 2 shows the minimum value of CURRENT_LSB is based on the maximum expected current, and directly defines the maximum resolution of the CURRENT register. While the smallest CURRENT_LSB value yields highest resolution, selecting a higher round-number (no higher than 8x) value for the CURRENT_LSB is common for simplifying the conversion of the CURRENT.
The RSHUNT term is the resistance value of the external shunt used to develop the differential voltage across the IN+ and IN– pins. Use Equation 1 for ADCRANGE = 0. For ADCRANGE = 1, the value of SHUNT_CAL must be divided by 4.
where
Note that the current is calculated following a shunt voltage measurement based on the value set in the SHUNT_CAL register. If the value loaded into the SHUNT_CAL register is zero, the current value reported through the CURRENT register is also zero.
After programming the SHUNT_CAL register with the calculated value, the measured current in Amperes can be read from the CURRENT register. Use Equation 3 to calculate the final value scaled by the CURRENT_LSB:

where
The power value can be read from the POWER register as a 16-bit value. Use Equation 4 to convert the power to Watts:
where
Refer to Detailed Design Procedure for a design example using these equations.