SBOS853C March 2017 – June 2025 OPT3001-Q1
PRODUCTION DATA
The PCB layout design for the OPT3001-Q1 device requires a couple of considerations. Bypass the power supply with a capacitor placed close to the OPT3001-Q1 device. Note that optically reflective surfaces of components also affect the performance of the design. The three-dimensional geometry of all components and structures around the sensor must be taken into consideration to prevent unexpected results from secondary optical reflections. Placing capacitors and components at a distance of at least twice the height of the component is typically sufficient. The most optimal optical layout is to place all close components on the opposite side of the PCB from the OPT3001-Q1 device. However, this approach is not practical for the constraints of every design.
Electrically connecting the thermal pad to ground is recommended. This connection can be created either with a PCB trace or with vias to ground directly on the thermal pad. If the thermal pad contains vias, the vias are recommended to be of a small diameter (< 0.2mm) to prevent the vias from wicking the solder away from the appropriate surfaces.
An example PCB layout with the OPT3001-Q1 device is shown in Figure 8-7.