SBVS442A December 2022 – October 2025 TPS748A
PRODUCTION DATA
By using the thermal metrics ΨJT and ΨJB, estimate the junction temperature with the following formulas. ΨJT and ΨJB are given in the Thermal Information table. For backwards compatibility, an older θJC(top) parameter is listed as well.

where:
For more information about measuring TT and TB, see the Using New Thermal Metrics application note, available for download at www.ti.com.
For a more detailed discussion of why TI does not recommend using θJC(top) to determine thermal characteristics, see the Using New Thermal Metrics application note. For further information, see the Semiconductor and IC Package Thermal Metrics application note. These application notes are also available on the TI website.