SCAT015 March   2025 TPUL2G123 , TPUL2G123-Q1 , TPUL2T122A , TPUL2T323

 

  1.   1
  2.   2
  3.   Trademarks

Overview

The TPUL family of monostable multivibrators is designed to be fully compatible with existing legacy monostable multivibrator offerings across multiple logic families from Texas Instruments. These new devices offer improved power consumption and accuracy while maintaining the same functionality, packages, and pinouts as the legacy devices.

Due to the unique output pulse timing non-linearity of each legacy device, which is influenced by process, voltage, temperature, and RC timing component variations, it is not possible to create a new device using a new technology node that perfectly matches any legacy device. Instead, the TPUL pulse generators target timing similarity with the majority of legacy devices. In most cases, replacing the timing resistor allows matching of the legacy device timing.

Device Comparison

The TPUL logic family is based on the latest technology from Texas Instruments, providing improvements to many existing families. The devices were designed to match or exceed performance for existing devices to provide the best transition from legacy devices to new devices in the majority of use cases.

Table 1 provides a quick reference table for replacing legacy devices with new TPUL function devices. Table 1 includes the expected pulse width error for a typical application if the external timing components are not modified, as well as the replacement resistor value to eliminate the error. These values are based on specific conditions: VCC = 5V, Rext = 10kΩ, and Cext = 0.1µF. The following sections provide more detailed explanations for designing the new TPUL devices into an existing system.

Table 1 Quick reference for device conversion
Legacy Device TPUL

Legacy

Output Pulse Width (two)

New

Output Pulse Width (two)

% Change

Rnew = Rold × Kold/Knew

(nearest 1% value) Ω

CD74HC123 2G123 450µs 886µs +98% 5062 (5.05k)
SN74LV123A 2G123 1ms 886µs -11% 11249 (11.3k)
SN74LV123A-Q1 2G123-Q1 1ms 886µs -11% 11249 (11.3k)
SN74AHC123A 2G123 1ms 886µs -11% 11249 (11.3k)
SN74AHCT123A 2T123 1ms 886µs -11% 11249 (11.3k)
CD74HCT123 2T123 1ms 886µs -11% 11249 (11.3k)
CD74HC423 2G122 450µs 886µs +98% 5062 (5.05k)
CD74HCT423 2T122 450µs 886µs +98% 5062 (5.05k)
CD14538 2G122A 995µs 886µs -11% 11192 (11.1k)
CD74HC4538 2G122A 700µs 886µs +27% 7874 (7.87k)
CD74HC4538-Q1 2G122A-Q1 700µs 886µs +27% 7874 (7.87k)
CD74HCT4538 2T122A 700µs 886µs +27% 7874 (7.87k)
CD74HC221 2G223 700µs 886µs +27% 7874 (7.87k)
SN74LV221A 2G223 1ms 886µs -11% 11249 (11.3k)
SN74LV221A-Q1 2G223-Q1 1ms 886µs -11% 11249 (11.3k)
CD74HCT221 2T223 700µs 886µs +27% 7874 (7.87k)
SN74123 2G123 250µs 886µs +256% 2812 (2.8k)
SN74LS123 2G123 250µs 886µs +256% 2812 (2.8k)

Table 2 provides a quick reference for comparing different logic family performance characteristics.

Table 2 Specification Comparison for Common Monostable Multivibrator Logic Families
Family
Specification HC HCT LV-A LS TTL (7400) CD4000 TPUL2G123
Supply voltage range 2V - 6V 4.5V - 5.5V 2V - 5.5V 4.75V - 5.75V 4.75V - 5.75V 3V - 18V 1.5V - 5.5V
Output drive current (5V) 4mA 4mA 12mA 8mA 16mA 1mA 12mA
Static supply current (max) 160µA 160µA 20µA 20mA 66mA 100µA 2µA
Active supply current (max) - - 975µA 20mA 66mA - 195µA

Modifying an Existing Design for Drop-In Replacement

The vast majority of designs only require a resistor value change to use the new TPUL family of logic. Some designs do not require any external component changes. The equation to change only a resistor is shown in Equation 1.

Equation 1. R n e w = K o l d K n e w R o l d

The K variable in Equation 1 comes from the monostable multivibrator pulse width equation, Equation 2. The K factor value can be found in the data sheet for each individual device and is dependent on multiple variables.

Equation 2. two=KRextCext

Steps to transition from legacy to TPUL:

  1. Identify the operational pulse width of the legacy device.
    1. Best practice is to measure in the existing system.
    2. Alternatively, refer to the legacy data sheet to determine the expected pulse width based on the timing component values.
  2. Identify the existing timing component values (Rext, Cext).
  3. Find the new expected pulse width using the original timing components and new TPUL device.
    1. The easiest method is to use the provided Excel-based calculator to get the expected pulse width. Example product folder: TPUL2G123
    2. The data sheet Application and Implementation section provides a method for calculating the expected pulse with without the provided calculator.
  4. If the expected pulse width from (3) is within the operational requirements of the system, a direct replacement is recommended. Stop here.
  5. Adjust timing components to match the desired pulse width.
    • The easiest method is to use the provided Excel-based calculator to get the required resistor and capacitor values to replace the existing components.
    • The alternate method is to adjust only the resistor using Equation 1.

Using the Provided Excel-Based Calculator

The Excel-based calculator is linked in each product folder under the Design & development section. This calculator provides three input methods.

The first method, shown in Figure 1, takes the supply voltage, timing resistor, and timing capacitor values and tolerances as inputs, and outputs the expected K Factor, nominal output pulse width, total pulse width range, and total error percentage. These values provide the system designer with important limitations of the accuracy of the TPUL device so that the designer can make informed decisions about the timing component selection. This view is particularly useful when timing components have been selected to provide a detailed look at the expected behavior in a system, especially when manufacturing at volume where tolerances play an important role in system requirements.

 Calculator Example for
                    Inputting Voltage and Component Values Figure 1 Calculator Example for Inputting Voltage and Component Values

The second method, shown in Figure 2, takes the supply voltage and desired output pulse width as inputs, and outputs the best options for the timing component values. If the Rext entry is blank, this means that the calculated value was outside the recommended range for the device. In particular, this view is helpful for selecting a resistor value to tune the timing for a particular application.

 Calculator Example for
                    Inputting Voltage and Desired Pulse Width Values Figure 2 Calculator Example for Inputting Voltage and Desired Pulse Width Values

The third method, shown in Figure 3, takes the timing resistor and capacitor values as inputs, and outputs the expected K Factor and pulse widths for each common voltage node between 1.5V and 5V. This view is particularly useful in observing variations in pulse width due to supply changes.

 Calculator Example for
                    Inputting Resistor and Capacitor Values Figure 3 Calculator Example for Inputting Resistor and Capacitor Values

These three methods are provided in the same Excel spreadsheet to give maximum flexibility to the system designer. In many cases, starting with method 2 allows a quick selection of the appropriate timing component values. Then, method 1 can be used to input industry standard component values and tolerances to get the best estimate of performance in the final system design.