SCDS390B September 2018 – March 2025 TMUX1511
PRODUCTION DATA
TON (VDD) time is defined as the time taken by the output of the device to rise to 90% after the supply has risen past the supply threshold. The 90% measurement is utilized to provide the timing of the device turning on in the system. The time constant from the load resistance and load capacitance can be added to the turn-on-VDD time to calculate system level timing. Figure 6-6 shows the setup used to measure transition time, denoted by the symbol tON (VDD).
TOFF (VDD) time is defined as the time taken by the output of the device to fall to 90% after the enable has fallen past the supply threshold. The 90% measurement is utilized to provide the timing of the device turning off in the system. The time constant from the load resistance and load capacitance can be added to the turn-off-VDD time to calculate system level timing. Figure 6-6 shows the setup used to measure transition time, denoted by the symbol tOFF (VDD).
Figure 6-6 Turn-On-VDD and Turn-Off-VDD Time Measurement Setup