The Home tab is displayed when launching the software. Connect the USB2ANY to the computer via a USB Cable. Make sure the USB2ANY is connected to the EVM with the cable inserted facing notch down to the EVM before using the GUI. If there is a successful connection, Hardware connected status will be shown at the bottom left corner of the GUI.
The Home tab includes SPI signal controls using eight toggle switches. Click on the toggle switch to turn on or off the channels.
Address mode turns on automatically when a switch is toggled. This mode can also turn on when the checkbox for Address mode is selected. Please note, when enabling Address mode by clicking on the checkbox, the first switch closes.
The Home Tab also shows a couple of buttons.
Sofware Reset and Clear Error Flags. The Sofware reset button writes two
commands consecutively to the register 0x0B: 1. 0xA3 2. 0x05. Clear
Error Falgs sends a 16-bit command 0x6CA9 to the TMUXS7614D.
From the Home tab, the user can access the
Registers Map and Daisy Chain Mode tabs. They are located on
the top left side of the screen in the white tab bar. The Registers Map
is symbolised by the pencil picture and the Daisy Chain Tab is the paper
sheet picture. They can be accessed by clicking on their symbol.
Figure 3-2 TMUXS7614D-SPI-EVM GUI Home Tab
Registers Map Tab
The Register Map allows toggling the switches in
address mode with a register viewpoint.
During operation, the Register Map updates the states of the registers,
while toggling the switches or triggering the error flags.
In daisy chain mode, the Register Map is not practical.