SCES221T April 1999 – August 2026 SN74LVC1G80
PRODUCTION DATA
For this application, a resistor needs to be placed on the feedback line for the initialization voltage from the microcontroller to overpower the signal coming from the output ( Q). Without it the state at the input will be challenged by the GPIO from the microcontroller and from the output of the SN74LVC1G80.
The SN74LVC1G80 device uses CMOS technology and has balanced output drive. Take care to avoid bus contention because it can drive currents that exceed maximum limits.