SCES885A April 2017 – August 2026 SN74LVC1G80-Q1
PRODUCTION DATA
For this application, a resistor needs to be placed on the feedback line for the initialization voltage from the microcontroller to overpower the signal coming from the output ( Q). Without it the state at the input will be challenged by the GPIO from the microcontroller and from the output of the SN74LVC1G80-Q1.
The SN74LVC1G80-Q1 device uses CMOS technology and has balanced output drive. Take care to avoid bus contention because it can drive currents that exceed maximum limits.