Some scenarios are listed below to
show the schedule is very tight.
- The schedule is delayed in the procedure before the cell is sent to TI. For example, the cell sample is delayed in the cell vendor side.
- The material of the cell has some
change after the cell has been sent to TI for Chem ID characterization. Need to
resend the new cell.
- Run into problems during
shipment, like custom clearance issue. There has previously been such a scenario
in the past.
In those cases, the schedule is very
tight. Users typically want to save as much time as possible, even one day.