SDAA074 July   2025 BQ27Z561 , BQ28Z610 , BQ40Z50

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Regular Process
    1. 1.1 Time Needed for Chem ID
    2. 1.2 Time Needed for Golden Learning
    3. 1.3 Time Needed for Low Temperature Test
  5. 2Scenarios for Very Tight Schedule
  6. 3How to Shorten the Time
  7. 4Summary
  8. 5References

Time Needed for Golden Learning

For the detailed steps of golden learning, refer to the Achieving the Successful Learning Cycle application note. The application note details the relax-charge-relax-discharge-relax test, and this can take approximately 1 day.

After golden learning, users need to run tests to verify the accuracy at room temp. This can take approximately 1 day.

If there is something wrong during the golden learning or accuracy test at room temp, then users need to run GPCRA to improve the room temp performance.

For detailed instructions, refer to the Simple Guide to GPC Golden GG Maker Tool application note.

After GPCRA, users need to also run a room temp accuracy test to verify if the performance is improved.