SDAA090 November 2025 INA234
A chopper-based CSA is constructed by wrapping a precision resistor gain network around a chopper stabilized OpAmp. One unique requirement of CSA is that common mode range must exceed supply voltage. This is done by decoupling the input common mode voltage and supply voltage. At high common mode, the input stage is powered through the common mode voltage source, or the bus voltage source that is being monitored by the CSA. This results in increased input bias current that must be supplied by the bus voltage source, even if the CSA is powered down.
The finite amount of current draw is typically not a problem. However, for low-power applications, or applications where only intermittent monitoring is required, one requirement is to reduce current draw as much as possible.The main goal of CCCSA is to reduce input bias current while preserving the advantages of chopping amplifier. Figure 2-1 shows the input stage of a CCCSA. Because there is no DC path between Vbus and the input of CCCSA, the DC input bias current is zero. Such devices make a viable option to satisfy the current sensing requirement in low-power applications.
For a traditional CSA, the input bias current (sum of both input+ and input-) can be as high as 100uA. Under the same condition, the input bias current of CCCSA is on the order of a few nA. Ultra-low input bias current not only enables low power application, this also enables convenient input low pass filtering without inflicting degradation in system accuracy.