SDAA158 December 2025 MSPM33C321A
For LVGL to properly perform animations and other tasks, LVGL requires a system tick, periodic timer triggers, and sleep management. Additional information on these requirements is listed below:
lv_tick_inc functional with the
amount of time elapsed in milliseconds. This can be done either in a timer
interupt or in the main while loop.lv_timer_handler periodically in a similar fashion to
the system tick. lv_tick_inc or lv_timer_handler, this
interupt must be stopped so that LVGL returns to the same state when the MCU
wakes up.