SDAA268 June 2026 ISO6431 , ISO6441
Figure 2-1 shows some TI examples of creepage and clearance values for reinforced, basic, and functional isolation, and different packages.
Figure 2-1 Some TI Example of Creepage,
Clearance and PackagingEngineers often get confused and there are some typical questions such as,
Figure 2-2 shows an example of key insulation specifications of ISO device and Table 2-1 lists the interpretation.
Figure 2-2 Key Insulation Specifications
Example of ISO Device| Parameter | Definition | Interpretation | Customer Key Concerns |
|---|---|---|---|
| Coordination/support safety standard | |||
| CLR | Clearance | The shortest distance between two conductive materials (pins) measured through air | Whether the CLR of the device meets the safety requirements of the customer's system |
| CPG | Creepage | The shortest distance between two conductive materials (pins) measured along the insulating surface | Whether the CPG of the device meets the safety requirements of the customer's system |
| CTI | Comparative Tracking Index | A parameter describing the difficulty of charge migration on the insulator surface, only related to the material itself. A higher value indicates the material surface is less prone to leakage. | The higher the CTI rating (higher voltage), the lower the creepage distance requirement |
| OVC | Overvoltage Category | The operating environment of mains-powered electrical equipment is divided into four overvoltage categories according to surge protection levels | Whether the OVC of the device meets the safety requirements of the customer's system |
| Component safety standard | |||
| VIORM | Maximum Repetitive Peak Isolation Voltage (VPK) | The maximum repetitive voltage (peak) that an isolated device must withstand during its lifetime | Parameters that isolated devices must meet under normal operation |
| VIOWM | Maximum Isolation Working Voltage (VRMS or VDC) | The maximum continuous working voltage (rms or DC) that an isolated device must withstand during its lifetime | |
| VIOTM | Maximum Transient Isolation Voltage (VPK) | The maximum transient voltage (usually non-repetitive) that an isolated device must withstand during its lifetime | Generally related to the actual required transient isolation voltage, operating bus voltage and corresponding OVC requirements |
| VIOSM | Maximum Surge Isolation Voltage (VPK) | The maximum peak voltage that an isolated device can withstand based on 1.2us/50us standard surge waveform | Characterizes the lightning surge voltage immunity |
Figure 2-3 shows the differences between clearance and creepage. About clearance, it's easy to understand that the shortest distance between two conductive materials (pins) is measured through air. However, for creepage, note that the shortest distance between two conductive materials (pins) is measured along the insulating surface. The insulating surface can be the chip top surface, side face or lower surface.
Figure 2-3 Clearance and Creepage
DifferencesGet back to those confusing questions in section 2.1, Does it mean that a reinforced isolated device can also make customer products reinforced? The answer is not always. Engineers must always differentiate component and system level insulation requirements.
Figure 2-4 shows a 1500V solar or ESS example for ISO-CAN design. Both ISO1050 and ISO1042 are reinforced ISO-CAN transceivers. However, the maximum isolation working voltage of ISO1050 is 1200V which can't satisfy isolation requirements in 1500V system.
Figure 2-4 1500V Solar or ESS Example for
ISO-CANTable 2-2 lists mandatory asked questions to select the ISO devices. They will be discussed in detail in section 3 to determine clearance and creepage distance.
| Question | Comments |
|---|---|
| 1. What is the system voltage (AC or DC)? | Used to determine CLR. |
| 2. What is the OVC? | |
| 3. Is it allowed to reduce the impulse withstand voltage by some methods (such as SPD)? | |
| 4. What is the pollution degree? | |
| 5. What is the maximum working altitude that the EE can support? | |
| 6. What is the working voltage (AC or DC)? | Used to determine CPG. |
| 7. What is the pollution degree and is potting acceptable to decrease it? | |
| 8. What is the CTI? |