To load the image in CCS, do the following steps:
- Before flashing the image, make sure
the erase configuration is set to Erase MAIN memory only.
- Load the binary. To do this select
run-> load->load program. Then select the generated out file.
- After loading the binary, there is an
error that Device Connection Error. This is expected as there is no code in 0x0 address.
Click ok first and try to reconnect the M33 core with Force Reset.
- After reconnecting to the M33 core,
users should find data in 0x00010000(non-secure image) in memory view.