SDAA498 September 2026 AM62L
The steps in this section assume that the user has a working TI SDK Yocto build environment for AM62Lx already set up. If you have not done this yet, follow the Building the SDK with Yocto guide first.
The expected directory layout after setup:
tisdk/
├── sources/ ← all layers live here
└── build/
└── conf/
├── bblayers.conf ← add extra layers here
└── local.conf ← add IMAGE_INSTALL / DISTRO_FEATURES / BBMASK hereAll
path references below use tisdk/ as the root.Build prerequisite: Before following any steps in this document, you must have sourced the Yocto build environment and completed at least one full image build (Step B — Section 2.6). These steps are prerequisites and must be done once:
cd tisdk/build
. conf/setenv
MACHINE=am62lxx-evm bitbake tisdk-default-imageThe environment source (. conf/setenv) must be re-run in every new terminal session before invoking bitbake or running any bitbake-based commands.