SFFS099 April   2021 ISO6741 , ISO6741-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 16-SOIC (wide-body SOIC) Package
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 16-DW (wide-body SOIC) Package

16-DW (wide-body SOIC) Package

Figure 4-1 shows the ISO6741/ISO6741-Q1 and ISO6741F/ISO6741F-Q1 pin diagram for the 16-DW package. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the ISO6741/ISO6741-Q1 data sheet.

GUID-821B0FA5-11B1-42F3-AE59-AA2298A6DA8A-low.gifFigure 4-1 Pin Diagram
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCC11No power to the device on side-1. Observe that the absolute maximum ratings for all pins of the device are met; otherwise device damage may be plausible. OUTD state undetermined.A
GND12Device continues to function as expected. D
INA3Input signal shorted to ground, so output (OUTA) stuck to low. Communication from INA to OUTA corrupted.B
INB4Input signal shorted to ground, so output (OUTB) stuck to low. Communication from INB to OUTB corrupted.B
INC5Input signal shorted to ground, so output (OUTC) stuck to low. Communication from INC to OUTC corrupted.B
OUTD6OUTD stuck low. Data communication from IND to OUTD lost. Device damage possible if IND is driven high for extended period of time.A
EN17Disables output buffer for OUTD. Communication corrupted for Channel D.B
GND18Device continues to function as expected. Normal operation.D
GND29Device continues to function as expected. Normal operation.D
EN210Disables the output buffer for OUTA/OUTB/OUTC channels. Communication corrupted.B
IND11Input signal shorted to ground, so output (OUTD) stuck to low. Communication from IND to OUTD corrupted.B
OUTC12OUTC stuck low. Data communication from INC to OUTC lost. Device damage possible if INC is driven high for extended period of time.A
OUTB13OUTB stuck low. Data communication from INB to OUTB lost. Device damage possible if INB is driven high for extended period of time.A
OUTA14OUTA stuck low. Data communication from INA to OUTA lost. Device damage possible if INA is driven high for extended period of time.A
GND215Device continues to function as expected. Normal operation.D
VCC216No power to the device on side-2. OUTA/OUTB/OUTC pins state undetermined.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCC11Operation undetermined. Either device is unpowered and OUTA/OUTB/OUTC=default logic state, OUTD=undetermined or through internal ESD diode on INA/INB/INC pin, device can power up if any IN is driven to logic high. If IN has current sourcing capability to provide regular operating current of device, ESD diode conducts that current and device damage plausible.A
GND12Device gets return ground through pin8. Normal operation.D
INA3No communication to INA channel possible. OUTA stuck to default state (High for ISO6741/ISO6741-Q1 and Low for ISO6741F/ISO6741F-Q1).B
INB4No communication to INB channel possible. OUTB stuck to default state (High for ISO6741/ISO6741-Q1 and Low for ISO6741F/ISO6741F-Q1).B
INC5No communication to INC channel possible. OUTC stuck to default state (High for ISO6741/ISO6741-Q1 and Low for ISO6741F/ISO6741F-Q1).B
OUTD6State of OUTD undetermined. Data communication from IND to OUTD lost.B
EN17Control on OUTD output buffer lost, but communication from IN to OUT channels continues normally.

B

GND18Device gets return ground through pin2. Normal operation.D
GND29Device gets return ground through pin15. Normal operation.D
EN210Control on OUTA/OUTB/OUTC output buffer lost, but communication from IN to OUT channels continues normally.

B

IND11No communication to IND channel possible. OUTD stuck to default state (High for ISO6741/ISO6741-Q1 and Low for ISO6741F/ISO6741F-Q1).B
OUTC12State of OUTC undetermined. Data communication from INC to OUTC lost.B
OUTB13State of OUTB undetermined. Data communication from INB to OUTB lost.B
OUTA14State of OUTA undetermined. Data communication from INA to OUTA lost.B
GND215Device gets return ground through pin9. Normal operation.D
VCC216Device unpowered on side-2 and state of OUTA/OUTB/OUTC undetermined.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
VCC1 1 GND1 No power to the device on side-1. Observe that the absolute maximum ratings for all pins of the device are met; otherwise device damage may be plausible. A
GND1 2 INA Input signal shorted to ground, so output (OUTA) stuck to low. Communication from INA to OUTA corrupted. B
INA 3 INB Communication corrupted for either INA or INB channel. B
INB 4 INC Communication corrupted for either INA or INB channel. B
INC 5 OUTD Communication corrupted for either or both channels. With opposite logic state on both channels, high current can flow between supply and ground and cause possible device damage. A
OUTD 6 EN1 Communication corrupted on Channel D. If EN1 is pulled to supply externally, possible device damage if OUTD driven low for extended duration. A
EN1 7 GND1 Disables OUTD output buffer. Communication for channel D corrupted. B
GND1 8 EN1 Already considered in above row. B
GND2 9 EN2 Disables the output buffer for all OUTA/OUTB/OUTC Output channels. Communication corrupted. B
EN2 10 IND Communication corrupted on Channel D if EN2 is pulled high or low externally. When IND toggles, communication corrupted on other channels whose output buffer is controlled by EN2. B
IND 11 OUTC Communication corrupted for either or both channels. With opposite logic state on both channels, high current can flow between supply and ground and cause possible device damage. A
OUTC 12 OUTB Communication corrupted for either or both channels. With opposite logic state on both channels, high current can flow between supply and ground and cause possible device damage. A
OUTB 13 OUTA Communication corrupted for either OUTA or OUTB channel. Device damage possible if INA and INB try to drive opposite logic state for extended duration creating a short between supply and ground on side-2. A
OUTA 14 GND2 OUTA stuck low. Data communication from INA to OUTA lost. Device damage possible if INA is driven high for extended period of time. A
GND2 15 VCC2 No power to the device on side-2. OUTA/OUTB/OUTC pins state undetermined. B
VCC2 16 GND2 Already considered in above row. B
Table 4-5 Pin FMA for Device Pins Short-Circuited to supply
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCC11No effect. Normal operation.D
GND12This can create potential difference between pin2 and pin8, causing high current to flow in device and potential device damage.A
INA3INA pin stuck high. Communication corrupted. OUTA state high.B
INB4INB pin stuck high. Communication corrupted. OUTB state high.B
INC5INC pin stuck high. Communication corrupted. OUTC state high.B
OUTD6OUTD stuck high. Data communication from INC to OUTC lost. Device damage possible if IND is driven low for extended period of time.A
EN17Functionality to disable output buffer OUTD lost. Communication for all channels normal.

B

GND18This can create potential difference between pin2 and pin8, causing high current to flow in device and potential device damage.A
GND29This can create potential difference between pin9 and pin15, causing high current to flow in device and potential device damage.A
EN210Functionality to disable output buffer for OUTA/OUTB/OUTC lost. Communication for all channels normal.

B

IND11IND pin stuck high. Communication corrupted. OUTD state high.B
OUTC12OUTC stuck high. Communication disrupted. If INC is low for extended duration, OUTC being stuck high creates a short and can damage the device.A
OUTB13OUTB stuck high. Communication disrupted. If INB is low for extended duration, OUTB being stuck high creates a short and can damage the device.A
OUTA14OUTA stuck high. Communication disrupted. If INA is low for extended duration, OUTA being stuck high creates a short and can damage the device.A
GND215This can create potential difference between pin9 and pin15, causing high current to flow in device and potential device damage.A
VCC216Device continues to function as expected. Normal operation.D