SFFS273 December 2021 LMK00804B-Q1
This section provides a failure mode analysis (FMA) for the pins of the LMK00804B-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the LMK00804B-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the LMK00804B-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| GND | 1 | No effect. Normal operation. | D |
| NC | 2 | Outputs disabled. | B |
| VDD | 3 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
| CLK_EN | 4 | CLK_EN pulled low. Outputs disabled to logic low state. | B |
| CLK_P | 5 | Invalid input clock. No output clocks if CLK_P/N input is selected. | B |
| CLK_N | 6 | Invalid input clock. No output clocks if CLK_P/N input is selected. | B |
| CLK_SEL | 7 | CLK_SEL pulled low. LVCMOS_CLK selected as input. | B |
| LVCMOS_CLK | 8 | Invalid input clock. No output clocks if LVCMOS_CLK input is selected. | B |
| GND | 9 | No effect. Normal operation. | D |
| Q3 | 10 | Output pulled low. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| VDDO | 11 | Outputs not functional. | B |
| Q2 | 12 | Output pulled low. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| GND | 13 | No effect. Normal operation. | D |
| Q1 | 14 | Output pulled low. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| VDDO | 15 | Outputs not functional. | B |
| Q0 | 16 | Output pulled low. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| GND | 1 | With this pin open, the device has a weaker ground connection than intended by design. Other ground pins maintain connection. Performance degradation possible. | C |
| NC | 2 | No effect. Normal operation. | D |
| VDD | 3 | Device unpowered. Device not functional. | B |
| CLK_EN | 4 | Internally pulled high. Outputs enabled. | D |
| CLK_P | 5 | Internally pulled low. No output clock. | B |
| CLK_N | 6 | Internally biased to VDD/2 when left floating. Normal operation for single ended input. | D |
| CLK_SEL | 7 | Internally pulled high. CLK_P, CLK_N (pins 5, 6) selected. | D |
| LVCMOS_CLK | 8 | The internal pulldown resistor ensures a low state when this input is left floating. | B |
| GND | 9 | With this pin open, the device has a weaker ground connection than intended by design. Other ground pins maintain connection. Performance degradation possible. | C |
| Q3 | 10 | No output. | C |
| VDDO | 11 | Outputs not powered. No output. | B |
| Q2 | 12 | No output. | C |
| GND | 13 | With this pin open, the device has a weaker ground connection than intended by design. Other ground pins maintain connection. Performance degradation possible. | C |
| Q1 | 14 | No output. | C |
| VDDO | 15 | Outputs not powered. No output. | B |
| Q0 | 16 | No output. | C |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|---|
| GND | 1 | NC | Outputs disabled. | B |
| NC | 2 | VDD | No effect. Normal operation. | D |
| VDD | 3 | CLK_EN | Pulled high. Outputs enabled. | D |
| CLK_EN | 4 | CLK_P | Not considered. Corner pin. | D |
| CLK_P | 5 | CLK_N | Clock input shorted. May create noise on output, if selected. | C |
| CLK_N | 6 | CLK_SEL | CLK_N pulled high. Potential duty cycle
distortion. CLK_SEL pulled high. CLK_P, CLK_N (pins 5, 6) selected. |
C |
| CLK_SEL | 7 | LVCMOS_CLK | Both pins pulled to Vdd/2. CLK_SEL will randomly selects LVCMOS_CLK or CLK_P/N. | B |
| LVCMOS_CLK | 8 | GND | Not considered. Corner pin. | D |
| GND | 9 | Q3 | Output pulled low. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| Q3 | 10 | VDDO | Output pulled high. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| VDDO | 11 | Q2 | Output pulled high. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| Q2 | 12 | GND | Not considered. Corner pin. | D |
| GND | 13 | Q1 | Output pulled low. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| Q1 | 14 | VDDO | Output pulled high. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| VDDO | 15 | Q0 | Output pulled high. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| Q0 | 16 | GND | Not considered. Corner pin. | D |
| Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
|---|---|---|---|
| GND | 1 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
| NC | 2 | No effect. Normal operation. | D |
| VDD | 3 | No effect. Normal operation. | D |
| CLK_EN | 4 | Pulled high. Outputs enabled. | D |
| CLK_P | 5 | If selected with CLK_SEL, input signal may not be recognized. | B |
| CLK_N | 6 | If selected with CLK_SEL, input signal may not be recognized. | B |
| CLK_SEL | 7 | Pulled high. CLK_P, CLK_N (pins 5, 6) selected. | D |
| LVCMOS_CLK | 8 | If input selected, outputs remain steady low or high. | B |
| GND | 9 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
| Q3 | 10 | Output pulled high. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| VDDO | 11 | No effect. Normal operation. | D |
| Q2 | 12 | Output pulled high. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| GND | 13 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
| Q1 | 14 | Output pulled high. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |
| VDDO | 15 | No effect. Normal operation. | D |
| Q0 | 16 | Output pulled high. No output clock. Long periods of high current flow through output transistors may cause device damage. | A |