SFFS310A April   2022  â€“ May 2022 TPS3704 , TPS3704-Q1

 

  1.   Trademarks
  2. 1Purpose of the Functional Safety Report
  3. 2Summary of Assessment
  4. 3Product Description
  5. 4Fulfillment of IEC 61508:2010 Requirements
  6. 5Fulfillment of ISO 26262:2018 Requirements
  7. 6Revision History

Fulfillment of ISO 26262:2018 Requirements

Texas Instruments carried out this assessment with respect to relevant requirements from the ISO 26262:2011 standard.

Table 5-1 Details of ISO 26262:2018 Requirements
ISO 26262:2011 Requirement Status Compliance Argument Evidence
Part 1: Vocabulary No requirements in this part N/A N/A N/A
Part 2: Management of Functional Safety a. Safety Culture Pass Texas Instruments maintains worldwide corporate policies related to; product and function safety; facility and materials safety, environment & health safety, risk and insurance management and customer satisfaction thru total qualify. These policies are implemented thru requirements and specification at the business units and factory level. Continuous improvement is integral to all processes. The semiconductor group has completed TUV certification of its processes for functional safety hardware and software development. TI Functional Safety Hardware development flow
Part 2: Management of Functional Safety b. Competence Management Pass Qualification and competence for the project safety manager is review during nomination of functional safety manager. Team members are assigned by their supervisors and supervisor ensure that the persons involved in the project execution have a sufficient level of skills, competencies and qualifications corresponding to their responsibilities. Documented Nomination of Functional Safety Manager
Part 2: Management of Functional Safety c. Quality Management Pass Texas Instruments sites first achieved the International Organization for Standardization´s (ISO) Quality Management System (ISO 9001) and Environmental Management System (ISO 14001) Certifications in 1996 and have maintained compliance to the ISO requirements since that time. TI is also TS 16949 certified; an international quality system standard specifically formulated for the global automotive industry. In addition, TI sites first achieved OHSAS 18001 certification in 2007, and has achieved Sony Green Partner certification Ti.com/Quality
Part 2: Management of Functional Safety d. Tailoring of the Safety Lifecycle Pass Functional safety process and deliverables are tailored by TI Functional Safety Hardware flow to be applied in addition to the requirements of the Automotive IC development process. The TI Functional Safety Hardware flow has been reviewed and certified by external assessors to satisfy the requirements For ISO-26262:2018 and IEC 61508:2010. TI Functional Safety Hardware development flow
Part 2: Management of Functional Safety e. Safety Management Pass Project manager and Safety manager were appointed to this project. Functional Safety Plan was generated and necessary audits and assessments were scheduled. Documentation of Nomination of Safety Manager
Part 2: Management of Functional Safety f. Functional Safety Plan Pass A functional safety plan was generated and followed throughout the project. Functional Safety Plan
Part 2: Management of Functional Safety g. Confirmation Measure Pass An independent confirmation measure of I3 performed the appropriate reviews and audits for this project. Documented Selection of Functional Safety Assessor, End of Phase Audits
Part 2: Management of Functional Safety h. Safety Management After Release to Production Pass A process is in place for handling safety management after release for production. Periodic Audit Report of Sustaining Operations, TI Quality Processes
Part 3: Concept Phase a. Item Definition N/A Requirements do not apply, however assumptions were made for the SEooC development. N/A
Part 3: Concept Phase b. Initiation of the Safety Lifecycle Pass Most requirements do not apply, however assumptions were made for the SEooC development. Additionally, a safety plan is generated for activities in the scope of the SEooC development. System Functional Safety Assumptions and Component Safety Requirements, Functional Safety Plan
Part 3: Concept Phase c. Hazard Analysis and Risk Assessment N/A Requirements do not apply, however assumptions were made for the SEooC development. N/A
Part 3: Concept Phase d. Functional Safety Concept Pass Most requirements do not apply, however assumptions were made for the SEooC development. System Functional Safety Assumptions and and Component Safety Requirements
Part 4: Product Development at a System Level not applicable for a hardware component SEooC development N/A N/A N/A
Part 5: Product Development at a Hardware Level a. Initiation of Product Development at the Hardware Level Pass In this hardware component SEooC development, the focus of the activities are around the requirements for product development at a hardware level. Documented Target Functional Safety Capability
Part 5: Product Development at a Hardware Level b. Specification of Hardware Safety Requirements Pass Hardware safety requirements have been generated from assumptions on the intended system. Target Functional Safety Capability, System Functional Safety Assumptions and Component Safety Requirements, SRS
Part 5: Product Development at a Hardware Level c. Hardware Design Pass Safety requirements have been incorporated into the design. Safety Analysis Report generated. Design Specification
Part 5: Product Development at a Hardware Level d. Evaluation of the Hardware Architectural Metrics N/A The requirements in this section are at the item level and do not apply to SEooC development. The calculations for the SEooC hardware component have been generated. Functional Safety Analysis Report
Part 5: Product Development at a Hardware Level e. Evaluation of Safety Goal Violations Due to Random Hardware Failures N/A The requirements in this section are at the item level and do not apply to SEooC development. The calculations for the SEooC hardware component have been generated. Functional Safety Analysis Report
Part 5: Product Development at a Hardware Level f. Hardware Integration and Testing N/A The requirements in this section are not applicable to SEooC development. N/A
Part 6: Product Development at a Software Level All sections N/A There are no software requirements for this SEooC development. N/A
Part 7: Production and Operation a. Production Pass Production details related to this SEooC are documented. The majority of the requirements in this section are not applicable to this SEooC development. Production Plan
Part 7: Production and Operation b. Operation, Service, and Decommissioning N/A The requirements in this section are not applicable to this SEooC development. N/A
Part 8: Supporting Processes a. Interfaces within distributed developments N/A The requirements in this section are not applicable to this SEooC development. A DIA is included in the Safety Manual for clarification of responsibilities. N/A
Part 8: Supporting Processes b. Specification and Management of Safety Requirements Pass Attention was given to safety requirements traceability throughout this project. System Functional Safety Assumptions and Component Safety Requirements, SRS, Functional Safety Plan
Part 8: Supporting Processes c. Configuration Management Pass Configuration management has been put in place for the work products created for this project. TI Functional Safety Hardware development process, Functional Safety Plan
Part 8: Supporting Processes d. Change Management Pass Change management requirements have been followed for this project and any changes that would impact safety have been addressed. Functional Safety Plan
Part 8: Supporting Processes e. Verification Pass Verification activities have been planned and executed. Verification Plans and Reports for each safety work product per Safety Plan
Part 8: Supporting Processes f. Documentation Pass This project follows TI Functional Safety Hardware documentation strategy. TI Functional Safety Hardware development flow, Functional Safety Plan
Part 8: Supporting Processes g. Confidence in Use of Software Tools Pass Software tool confidence has been documented. Software Tool Plan
Part 8: Supporting Processes h. Qualification of Software Components N/A Software components are not an aspect of this product. N/A
Part 8: Supporting Processes i. Qualification of Hardware Components Pass IC was qualified per AEC-Q100 requirements. Qualification requirements related to the applicability of the IC to be integrated into the system do not apply to SEooC development. Qualification Plan and Report
Part 8: Supporting Processes j. Proven in Use Argument N/A Proven in use argument is not claimed. N/A
Part 9: ASIL Analysis a. Requirements Decomposition N/A ASIL requirements were not decomposed. N/A
Part 9: ASIL Analysis b. Criteria for Coexistence of Elements N/A No coexisting requirements N/A
Part 9: ASIL Analysis c. Analysis of Dependent Failures Pass Dependent failure analysis was considered at the hardware component level. Dependent Failure Analysis
Part 9: ASIL Analysis d. Safety Analysis Pass FMEA, FMEDA, FIT calculations and others are included for the hardware component. Functional Safety Analysis Report
Part 10: Guideline on ISO 26262 No requirements in this part N/A ISO 26262-10 is an informative reference. There are no requirements in ISO 26262-10, however the work products and analysis techniques that are recommended by this part are incorporated into the TI Functional Safety Hardware development flow and work product templates that have been used for this project. N/A
Part 11: Guidelines on Application of ISO 26262 to semiconductors No requirements in this part N/A ISO 26262-11 is an informative reference. There are no requirements in ISO 26262-11, however the work products and analysis techniques that are recommended by this part are incorporated into the TI Functional Safety Hardware development flow and work product templates that have been used for this project. N/A
Part 12: Adaption of ISO 26262 to Motorcycles All sections N/A The tables of ISO 26262-12 only apply at the system level for motorcycles, they do not apply to a hardware component SEooC. These tables are the responsibility of the system integrator if applicable. N/A