SFFS983A August 2025 – October 2026 MSPM0G1518 , MSPM0G1519 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0G3529-Q1
This checks the plausibility of inputs being sampled by ADC. For example, if information is related to:
Checks can be performed to see if the readings meet these plausibility conditions. In addition to doing checks on the ADC output, the time duration from the last interrupt can be checked in software and compared against the expected ADC sampling rate. If the duration from the last interrupt is beyond the acceptable range, corrective actions can be taken.