SFFSAU3 August   2026 LM851772-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the LM851772-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the LM851772-Q1 pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the LM851772-Q1 datasheet.

LM851772-Q1 Pin Diagram Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • The device is used within the Recommended Operating Conditions and the Absolute Maximum Ratings found in the LM851772-Q1 datasheet.
  • For the analysis, the typical application with VI = 9V to 48V, VO = 20V and PO = 100W shown in the Typical Application section of the LM851772-Q1 datasheet is considered.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VCC1 1 When the VCC1 pin is disabled through logic and connected through a resistor to GND: There is no impact to the device. D
When the VCC1 pin is disabled through logic and connected to the VCC2 pin: The device does not start. B
When the VCC1 pin is enabled: VCC1 operates in current limit at 0V. B
SS/ATRK 2 The device regulates the output voltage to 0V. B
SYNC 3 When the SYNC pin is not used and connected to GND: There is no effect to the device. D
When the SYNC pin is not used and connected to the VCC2 pin: The device does not start. B
When the SYNC pin is configured as the clock input signal: There is no SYNC functionality. C
When the SYNC pin is configured as the clock output signal: There is no SYNC signal available to the other phase. C
DTRK 4 When the DTRK pin is used: There is a loss of the functionality of DTRK, the device regulates to the internal reference. B
When the DTRK pin is not used and connected to GND: There is no effect to the device. D
When the DTRK pin is not used and connected to the VCC2 pin: The device does not start. B
SDA 5 Communication with the device is not possible. B
SCL 6 Communication with the device is not possible. B
MODE 7 Power save mode is enabled. C
When the MODE pin is connected to the VCC2 pin: The device does not start. B
CFG2 8 When the CFG2 pin is used at nRST rise: There is a possible configuration change from the expected configuration to configuration 1, see the CFG2 Pin (R2D-CH2) Configuration Overview table in the datasheet. C
When the CFG2 pin is used after start-up: There is no effect to the device. D
ADDR(CFG1) 9 When the ADDR(CFG1) pin is shorted at nRST rise: I2C is enabled, the device address is set to 0x6A, and the slope compensation is set according configuration 1, see the ADDR Pin (R2D-CH1 Configuration Overview table in the datasheet. C
When the ADDR(CFG1) pin is shorted after start-up: There is no effect to the device. D
CDC 10 When the CDC pin is configured as current monitor: There is no output signal. B
When the CDC pin is configured as cable drop compensation: There is no load current dependent offset on the output voltage of the converter. B
When the CDC pin is disabled: There is no impact to the device. D
nFLT/nINT 11 The pin permanently indicates a fault or interrupt. B
RT 12 The converter switches at maximum frequency (≅2.5MHz). B
COMP 13 If the MODE pin is low: The converter does not switch. B
If the MODE pin is high: The inductor current goes to the negative current limit until IVP is triggered. B
FB/SEL_intFB 14 With external feedback (FB): The output voltage rises until the device triggers overvoltage protection. B
When the internal FB is used, and the pin is connected to the VCC2 pin: The device does not start. B
AGND 15 There is no effect to the device. The device operates normally. D
ILIMCOMP 16 The pin is used: The current loop is unstable, or the average current limit is not available. C
The pin is connected to the VCC2 pin: The device does not switch. B
AGND 17 There is no effect to the device. The device operates normally. D
VOUT 18 The converter operates in peak or average current limit and the output voltage is shorted to GND. B
ISNSN 19 The differential voltage on the sense amplifier is too high. Potential damage to the pin. A
ISNSP 20 The differential voltage on the sense amplifier is too high. Potential damage to the pin. A
CSB 21 The differential voltage on the sense amplifier is too high. Potential damage to the pin. A
CSA 22 The differential voltage on the sense amplifier is too high. Potential damage to the pin. A
SW1 23 There is no output voltage. Potential damage to the device. A
HO1 24 There is no output voltage. The buck high-side FET is off. B
HB1 25 There is no supply for the gate driver. The device is in standby (BOOT_UV). B
NC 26 There is no effect to the device. The device operates normally. D
LO1 27 The operation is non-synchronous in buck-mode and partially in buck-boost mode. Potential damage to the external FET due to power dissipation. C
PGND 28 There is no effect to the device. The device operates normal. D
VCC2 29 The device does not start. B
LO2 30 The boost low-side FET is always off. There is no boost operation. C
HB2 31 There is no supply for the gate driver. The device is in standby (BOOT_UV). B
HO2 32 The operation is non-synchronous in boost-mode and partially in buck-boost mode. Potential damage to the external FET due to power dissipation. C
SW2 33 There is no output voltage. Potential damage to the device. A
NC 34 There is no effect to the device. The device operates normal. D
DRV1 35 When DRV1 is used: There is no system output. B
When DRV1 is not used: There is no effect to the device. D
BIAS 36 There is no effect to the device. The efficiency of the converter is potentially reduced, or the thermal shutdown triggers. C
EN/UVLO 37 The device is in shutdown or standby. B
nRST 38 The device is in shutdown. B
NC 39 There is no effect to the device. The device operates normal. D
VIN 40 The device is in shutdown or standby. B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VCC1 1 When the VCC1 pin is disabled: There is no impact to the device. D
When the VCC1 pin is enabled: VCC1 oscillates. Potential damage to the device. A
SS/ATRK 2 There is a rapid start-up with potentially high inrush current to the converter. C
SYNC 3 Unstable switching frequency is possible. C
DTRK 4 Erratic operation is possible. B
SDA 5 Communication with the device is not possible. B
SCL 6 Communication with the device is not possible. B
MODE 7 PSM/FPWM is undefined. C
CFG2 8 When the open happens before nRST rise: At nRST rise, the configuration of the device is undefined. C
When the CFG2 pin open happens after start-up: There is no effect to the device. D
ADDR (CFG1) 9 When the ADDR(CFG1) pin open happens before nRST rise: At nRST rise, the address and configuration of the device is undefined. C
When the ADDR(CFG1) pin open happens after start-up: There is no effect to the device. D
CDC 10 When the CDC pin is configured as current monitor: There is no signal to the system. C
When the CDC pin is configured as cable drop compensation: The maximum offset on the output is undefined and independent of the load current. B
When the CDC pin is disabled: There is no impact to the device. D
nFLT/nINT 11 The pin does not indicate a fault or interrupt. B
RT 12 The lowest switching frequency is selected and the converter is potentially unstable. C
COMP 13 The voltage loop is unstable. Potential damage to external components or the device. A
FB/SEL_intFB 14 The output voltage is regulated to the overvoltage protection (OVP) level or 0V. B
AGND 15 Increased current flow at the internal AGND/PGND connection. The operation is potentially erratic. Potential damage to the device. A
ILIMCOMP 16 The current loop is unstable. C
AGND 17 Increased current flow at the internal AGND/PGND connection. The operation is potentially erratic. Potential damage to the device. A
VOUT 18 With an internal FB divider: There is no regulation of the output voltage. Potential damage to external components or the device. A
With an external FB divider: There is no overvoltage protection (OVP), and no slope compensation. Potential unstable current loop. B
ISNSN 19 If the average current function is not used, there is no effect to the device. D
There is no average current limit function. B
ISNSP 20 If the average current function is not used, there is no effect to the device. D
There is no average current limit function. B
CSB 21 There is erratic switching behavior. There is a loss of regulation. Potential damage to the device or external components. A
CSA 22 There is erratic switching behavior. There is a loss of regulation. Potential damage to the device or external components. A
SW1 23 There is a loss of operation or regulation, or the device turns off. B
HO1 24 There is no output voltage. The buck high-side FET is off. B
HB1 25 There is no supply for the gate driver. The device is in standby (BOOT_UV). B
NC 26 There is no effect to the device. The device operates normal. D
LO1 27 The operation is non-synchronous in buck-mode and partially in buck-boost mode. Potential damage to the external FET due to power dissipation. C
PGND 28 Increased current flow at the internal AGND/PGND connection. The operation is potentially erratic. Potential damage to the device. A
VCC2 29 The internal supply us unstable. The operation is erratic. B
LO2 30 The boost low-side FET is always off, no boost operation. B
HB2 31 There is no supply for the gate driver. The device is in standby (BOOT_UV). B
HO2 32 The operation is non-synchronous in boost-mode and partially in buck-boost mode. Potential damage to the external FET due to power dissipation. C
SW2 33 There is a loss of operation, or the device turns off. B
NC 34 There is no effect to the device. The device operates normal. D
DRV1 35 When the DRV1 pin is used: There is no output voltage to the load B
When the DRV1 pin is not used: There is no effect to the device. D
BIAS 36 The efficiency of the device is potentially reduced, or there is a thermal shutdown. C
EN/UVLO 37 The device turns on or off unpredictably. B
nRST 38 The device turns on or off unpredictably. B
NC 39 There is no effect to the device. The device operates normal. D
VIN 40 The device is not supplied. The device does not start-up. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
VCC1 1 SS/ATRK (2) When the VCC1 pin is enabled: There is no functionality of SS/ATRK. C
When the VCC1 pin is disabled and tied to GND: The output is regulated to 0V. B
When the VCC1 pin is disabled and tied to the VCC2 pin: There is no functionality of SS/ATRK. C
SS/ATRK 2 SYNC (3) When the SYNC pin is connected to GND: The device does not start-up. B
When the SYNC pin is connected to the VCC2 pin: There is no functionality of SS/ATRK. C
When the SYNC pin is driven from external signal: Functionality is erratic. B
When the SYNC pin is configured as output: The output voltage is modulating with the SYNC signal. B
SYNC 3 DTRK (4) When the SYNC and DTRK pins are connected to the same signal: There is no effect to the device. D
When the SYNC or DTRK pins are driven from an external signal: The output voltage and frequency are modulated with the external signal. B
When the SYNC pin is configured as output: The output voltage of the converter is at 50% due to the DTRK functionality. B
DTRK 4 SDA (5) The output voltage is potentially modulated with the I2C communication or no I2C communication possible. B
SDA 5 SCL (6) No I2C communication possible, so the device does not start-up. B
SCL 6 MODE (7) No I2C communication possible, so the device does not start-up. B
MODE 7 CFG2 (8) When nRST rises: Configuration 1 or 16 are selected depending on the voltage at MODE pin. B
The short is applied after start-up: The PFM or FPWM selection is unclear. B
When one pin is connected to VCC2, and the other pin is connected to GND: The device does not start. B
CFG2 8 ADDR(CFG1) (9) The setting of the ADDR(CFG1) pin defines if the device is operating in configuration 1 or 16, see the datasheet. B
When the short is applied after start-up: There is no effect to the device. D
When one pin is connected to the VCC2 pin, and the other pin is connected to GND: The device does not start. B
ADDR(CFG1) 9 CDC (10) When ADDR(CFG1) is connected to GND, see the pin to GND short table. B
D
When ADDR(CFG1) is connected to VCC2 and the CDC pin is configured as current monitor: The system gets a current signal indicated that is at the highest possible level independent of the real value measured. B
When ADDR(CFG1) is connected to VCC2 and the CDC pin is configured as cable drop compensation: The maximum offset on the output is undefined and independent of the load current. B
When ADDR(CFG1) is connected to VCC2 and the CDC pin is disabled (and connected to GND), see the pin to GND short table. C
D
CDC 10 nFLT/nINT (11) If a pullup is connected to the nFLT/nINT pin and the CDC pin is configured as cable drop compensation: The output voltage is somewhat higher than set by the measured output current. C
If a pullup is connected to the nFLT/nINT pin and the CDC pin is configured as current monitor: The system gets a current signal indication that is higher than the measured output current. C
If the CDC pin is disabled (and connected to GND), the nFLT/nINT permanently indicates a fault. B
nFLT/nINT 11 RT (12) If a pullup is connected to the nFLT/nINT pin: The switching frequency decreases. C
Whenever the nFLT/nINT pin is pulled low, the converter operates at maximum switching frequency and is potentially unstable. B
RT 12 COMP (13) The switching frequency is unstable. The voltage loop is potentially unstable. B
COMP 13 FB/SEL_intFB (14) When there is an external FB divider: The operation is erratic. B
When there is an internal FB divider, and the pin is connected to the VCC2 pin: The operation is in current limit until OVP is triggered. B
FB/SEL_intFB 14 AGND (15) See the pin to GND short table. B
AGND 15 ILIMCOMP (16) See the pin to GND short table. B
C
ILIMCOMP 16 AGND (17) See the pin to GND short table. B
C
AGND 17 VOUT (18) The converter operates in peak or average current limit and the output voltage is shorted to GND. B
VOUT 18 ISNSN (19) When the ISNSN pin is connected to GND: The device operates in peak or average current limit and the output voltage is shorted to GND. B
With input sensing: The differential voltage on the ISNSx pin is potentially too high. A
With output sensing: The average current limit (sense line shorted) is potentially inaccurate. C
ISNSN 19 ISNSP (20) There is no average current limit function. B
ISNSP 20 CSB (21) The differential voltage on the sense amplifier is too high. Potential damage to one of the pins. A
CSB 21 CSA (22) There is no peak current limit function. B
CSA 22 SW1 (23) The peak current limit (sense line shorted) is potentially inaccurate. C
SW1 23 HO1 (24) The device is in standby (BOOT_UV). B
HO1 24 HB1 (25) The device is in standby (BOOT_UV). B
HB1 25 NC (26) There is no effect to the device. The device operates normal. D
NC 26 LO1 (27) There is no effect to the device. The device operates normal. D
LO1 27 PGND (28) The operation is non-synchronous in buck-mode and partially in buck-boost mode. Potential damage to the external FET due to power dissipation. C
PGND 28 VCC2 (29) The device does not start. B
VCC2 29 LO2 (30) The device is in standby or shuts down. (The VCC2 pin is pulled to ground when the LO2 pin is pulled low.) B
LO2 30 HB2 (31) At start-up the device stays in standby (BOOT_UV). B
After start-up potential damage due to overvoltage on pin LO2. A
HB2 31 HO2 (32) The device is in standby (BOOT_UV). B
HO2 32 SW2 (33) The device is in standby (BOOT_UV). B
SW2 33 NC (34) There is no effect to the device. The device operates normally. D
NC 34 DRV1 (35) There is no effect to the device. The device operates normally. D
DRV1 35 BIAS (36) The external disconnect FET is potentially damaged. A
BIAS 36 EN/UVLO (37) There is a loss of the control of the EN/UVLO pin, and the device is in standby or the device is on. B
EN/UVLO 37 nRST (38) There is a loss of the control of the EN/UVLO pin, and the device is in standby or the device is on. C
nRST 38 NC (39) There is no effect to the device. The device operates normal. D
NC 39 VIN (40) There is no effect to the device. The device operates normal. D
VIN 40 VCC1 (1) There is device damage due to high voltage on pin VCC1. A
Table 4-5 Pin FMA for Device Pins Short-Circuited to VIN
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
VCC1 1 There is device damage due to high voltage. A
SS/ATRK 2 There is device damage due to high voltage. A
SYNC 3 There is device damage due to high voltage. A
DTRK 4 There is device damage due to high voltage. A
SDA 5 There is device damage due to high voltage. A
SCL 6 There is device damage due to high voltage. A
MODE 7 There is device damage due to high voltage. A
CFG2 8 There is device damage due to high voltage. A
ADDR(CFG1) 9 There is device damage due to high voltage. A
CDC 10 There is device damage due to high voltage. A
nFLT/nINT 11 There is device damage due to high voltage. A
RT 12 There is device damage due to high voltage. A
COMP 13 There is device damage due to high voltage. A
FB/SEL_intFB 14 There is device damage due to high voltage. A
AGND 15 There is device damage due to high voltage to PGND. A
ILIMCOMP 16 There is device damage due to high voltage. A
AGND 17 There is device damage due to high voltage to PGND. A
VOUT 18 The converter is bypassed. B
ISNSN 19 With input sensing: There is no average current limit. B
With output sensing: The differential voltage between the ISNSP and ISNSN pins is potentially too high. A
ISNSP 20 With input sensing: The input sensing (sense line shorted) is inaccurate. C
With output sensing: The differential voltage between the ISNSP and ISNSN pins is potentially too high. A
CSB 21 The buck high-side FET is bypassed. The operation is erratic. There is potentially damage to the device due to high differential voltage between the CSA and CSB pins. A
CSA 22 The buck high-side FET is bypassed. The operation is erratic. There is potentially damage to the device due to high differential voltage between the CSA and CSB pins. A
SW1 23 The buck high-side FET is bypassed. The operation is erratic. B
HO1 24 There is device damage due to high voltage. A
HB1 25 There is device damage due to high voltage. A
NC 26 There is no effect to the device. The device operates normal. D
LO1 27 There is device damage due to high voltage. A
PGND 28 There is device damage due to high voltage to AGND. A
VCC2 29 There is device damage due to high voltage. A
LO2 30 There is device damage due to high voltage. A
HB2 31 There is device damage due to high voltage. A
HO2 32 There is device damage due to high voltage. A
SW2 33 The boost low-side FET is potentially damaged. B
NC 34 There is no effect to the device. The device operates normal. D
DRV1 35 The external disconnect FET is potentially damaged. B
BIAS 36 When the BIAS pin is connected to the VOUT pin: VIN and VOUT are shorted. B
When the BIAS pin is connected to VIN: There is no effect to the device. D
EN/UVLO 37 There is no UVLO function. The nRST pin defines standby and enable. D
nRST 38 The nRST pin is always enabled. D
NC 39 There is no effect to the device. The device operates normal. D
VIN 40 There is no effect to the device. The device operates normal. D