SFFSBD9 June 2026 TPS7E81-Q1
Figure 4-3 shows the TPS7E81-Q1 pin diagram for the DGN (HVSSOP, 8) package. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS7E81-Q1 datasheet.
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN | 1 | There is no power supplied to the device; resulting in no output voltage. | B |
| EN | 2 | The device is stuck in shutdown mode; resulting in no output voltage. | B |
| NC | 3 | There is no effect on the device. The device operates as normal. | D |
| GND | 4 | There is no effect on the device. The device operates as normal. | D |
| GND | 5 | There is no effect on the device. The device operates as normal. | D |
| NC | 6 | There is no effect on the device. The device operates as normal. | D |
| NC/ADJ | 7 | Fixed output: There is no effect on the device. The device operates as normal. | D |
| Adjustable output: The device operates in dropout mode. VOUT follows VIN and equals VIN - VDO. | B | ||
| OUT | 8 | The device is not operational with the output being pulled to GND. Current limit is triggered, and the device potentially repeats entering and exiting thermal shutdown depending on power dissipation. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN | 1 | There is no power supplied to the device; resulting in no output voltage. | B |
| EN | 2 | The device has an internal pullup, and therefore, remains enabled. The device operates as normal unless the user attempts to disable the device. | D |
| B | |||
| NC | 3 | There is no effect on the device. The device operates as normal. | D |
| GND | 4 | There is no effect on the device. The device operates as normal since the device has an additional ground pin. | D |
| GND | 5 | There is no effect on the device. The device operates as normal since the device has an additional ground pin. | D |
| NC | 6 | There is no effect on the device. The device operates as normal. | D |
| NC/ADJ | 7 | Fixed output: There is no effect on the device. The device operates as normal. | D |
| Adjustable output: The input of the error amplifier is not connected, leaving VOUT in an indeterminate state. | B | ||
| OUT | 8 | The device does not provide a regulated rail and is disconnected from the load. | B |
| Pin Name | Pin No. | Shorted to | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|---|
| IN | 1 | EN | 2 | The EN pin is pulled to the IN supply. Shutdown mode is not possible. The device is powered on as long as the input supply is present. | D |
| B | |||||
| EN | 2 | NC | 3 | There is no effect on the device. The device operates as normal. | D |
| NC | 3 | GND | 4 | There is no effect on the device. The device operates as normal. | D |
| GND | 4 | NC | 5 | There is no effect on the device. The device operates as normal. | D |
| NC | NC/ADJ | Fixed output: There is no effect on the device. The device operates as normal. | D | ||
| Adjustable output: There is no effect on the device. The device operates as normal. | D | ||||
| NC/ADJ | OUT | Fixed output: There is no effect on the device. The device operates as normal. | D | ||
| Adjustable output: The feedback network is bypassed and the device operates in unity gain configuration. VOUT = Internal Bandgap VREF. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| IN | 1 | The device operates as normal if already operating off-battery. If operating post-regulator, there is potentially increased power dissipation across the device and this potentially results in thermal shutdown. | D |
| B | |||
| EN | 2 | The device remains enabled and survives the fault condition. The device operates as normal unless the user attempts to disable the device. | D |
| B | |||
| NC | 3 | There is no effect on the device. The device operates as normal. | D |
| GND | 4 | At a system level, this results in a flow of large currents and possible collapse of the input voltage to the LDO. In this type of scenario, there is no LDO output voltage. | B |
| GND | 5 | At a system level, this results in a flow of large currents and possible collapse of the input voltage to the LDO. In this type of scenario, there is no LDO output voltage. | B |
| NC | 6 | There is no effect on the device. The device operates as normal. | D |
| NC/ADJ | 7 | Fixed output: There is no effect on the device. The device operates as normal. | D |
| Adjustable output: This violates the absolute maximum rating of the ADJ pin and damages the device. | A | ||
| OUT | 8 | If operating off-battery, the device survives this fault condition but does not provide a regulated rail. If operating post-regulator, this results in a flow of reverse current and damages the device. | B |
| A |