SFFSBP4 November 2026 TLIN829-Q1
Figure 4-1 shows the TLIN829-Q1 pin diagram for the SOIC (D, 8) package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TLIN829-Q1 datasheet.
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| RXD | 1 | The RXD pin is biased dominant; communication from the LIN bus to the MCU is not possible. | B |
| EN | 2 | The device potentially only operates in standby mode after power-on. If a short occurs in normal mode, the part is forced to enter sleep mode and potentially disables LIN communication. | B |
| NC | 3 | NC is not connected and has no effect on device behavior. | D |
| TXD | 4 | The TXD pin is biased dominant; communication from the MCU to the LIN bus is not possible. | B |
| GND | 5 | None. | D |
| LIN | 6 | The LIN pin is biased dominant; LIN communication is not possible. | B |
| VSUP | 7 | The device is not powered and does not function. | B |
| NC | 8 | NC is not connected and has no effect on device behavior. | D |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| RXD | 1 | Communication from the LIN bus to the MCU is not possible. | B |
| EN | 2 | The EN pin is biased low due to internal pulldown, so the device is in standby mode. | B |
| NC | 3 | NC is not connected and has no effect on device behavior. | D |
| TXD | 4 | Communication from the MCU to the LIN bus is not possible. | B |
| GND | 5 | The device is not powered and does not function. | B |
| LIN | 6 | LIN communication is not possible. | B |
| VSUP | 7 | The device is not powered and does not function. | B |
| NC | 8 | NC is not connected and has no effect on device behavior. | D |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| RXD | 1 | EN | The device goes into sleep mode when a dominant bit is received on the LIN bus, disabling communication. | B |
| EN | 2 | NC | NC is not connected and has no effect on device behavior. | D |
| NC | 3 | TXD | NC is not connected and has no effect on device behavior. | D |
| GND | 5 | LIN | The LIN pin is biased dominant, LIN communication is not possible. | B |
| LIN | 6 | VSUP | The LIN pin is biased recessive, LIN communication is not possible. | B |
| VSUP | 7 | NC | NC is not connected and has no effect on device behavior. | D |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| RXD | 1 | There is an absolute maximum voltage violation, and the transceiver is potentially damaged. | A |
| EN | 2 | There is an absolute maximum voltage violation, and the transceiver is potentially damaged. | A |
| NC | 3 | NC is not connected and has no effect on device behavior. | D |
| TXD | 4 | There is an absolute maximum voltage violation, and the transceiver is potentially damaged. | A |
| GND | 5 | The device is not powered and does not function. | A |
| LIN | 6 | The LIN pin is biased recessive, LIN communication is not possible. | B |
| VSUP | 7 | None | D |
| NC | 8 | NC is not connected and has no effect on device behavior. | D |