SFFSBP4 November   2026 TLIN829-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 SOIC (D, 8) Package
    2. 2.2 VSON (DRB, 8) Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 SOIC (D, 8) Package
    2. 4.2 VSON (DRB, 8) Package
  7. 5Revision History

VSON (DRB, 8) Package

Figure 4-2 shows the TLIN829-Q1 pin diagram for the VSON (DRB, 8) package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TLIN829-Q1 datasheet.

TLIN829-Q1 Pin Diagram (DRB Package, 8-Pin (VSON) Package)Figure 4-2 Pin Diagram (DRB Package, 8-Pin (VSON) Package)
Table 4-6 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
RXD1The RXD pin is biased dominant; communication from the LIN bus to the MCU is not possible.B
EN2The device potentially only operates in standby mode after power-on. If a short occurs in normal mode, the part is forced to enter sleep mode and potentially disables LIN communication.B
WAKE3The WAKE pin is biased to ground and a local wake up is not possible.B
TXD4The TXD pin is biased dominant; communication from the MCU to the LIN bus is not possible.B
GND5NoneD
LIN6The LIN pin is biased dominant; LIN communication is not possible.B
VSUP7The device is not powered and does not function.B
INH8The INH pin is biased to GND and is not able to enable system power if used in this manner.B
Note: The DRB package includes a thermal pad.
Table 4-7 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
RXD1Communication from the LIN bus to the MCU is not possible.B
EN2The EN pin is biased low due to internal pulldown, so the device is in standby mode.B
WAKE3Local wake up is not possible.B
TXD4Communication from the MCU to the LIN bus is not possible.B
GND5The device is not powered and does not function.B
LIN6LIN communication is not possible.B
VSUP7The device is not powered and does not function.B
INH8The INH pin is not able to enable system power if used in this manner.B
Note: The DRB package includes a thermal pad.
Table 4-8 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure EffectsFailure Effect Class
RXD1ENThe device goes into sleep mode when a dominant bit is received on the LIN bus, disabling communication.B
EN2WAKEThe absolute maximum voltage on the EN pin is potentially exceeded causing damage to EN pin.A
WAKE3TXDThe absolute maximum voltage on the WAKE pin is potentially exceeded causing damage to TXD pin.A
GND5LINThe LIN pin is biased dominant, LIN communication is not possible.B
LIN6VSUPThe LIN pin is biased recessive, LIN communication is not possible.B
VSUP7INHThe INH pin is biased high and is not able to turn off system power if used in this manner.B
Note: The DRB package includes a thermal pad. When the thermal pad is soldered down, there is a possibility that the pad can short to any pin on the device. The behavior of the device in this failure condition is determined by what the thermal pad is connected to. Example: If the thermal pad is soldered to a ground plane, then the adjacent pins behave as if shorted to ground.
Table 4-9 Pin FMA for Device Pins Short-Circuited to VSUP Supply
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
RXD1There is an absolute maximum voltage violation, and the transceiver is potentially damaged.A
EN2There is an absolute maximum voltage violation, and the transceiver is potentially damaged.A
WAKE3The WAKE pin is biased high and a local wake up is not possible.B
TXD4There is an absolute maximum voltage violation, and the transceiver is potentially damaged.A
GND5The device is not powered and does not function.A
LIN6The LIN pin is biased recessive, LIN communication is not possible.B
VSUP7NoneD
INH8The INH pin biased high and is not able to turn off system power if used in this manner.B
Note: The DRB package includes a thermal pad.