SFFSBP7 November 2026 TPS1HTC100-Q1
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| GND | 1 | The resistor diode network is bypassed if present. | B |
| EN | 2 | There is a shutdown of the output. | B |
| DIAG_EN | 3 | The diagnostics are disabled. | B |
| FAULT | 4 | The reported status can be erroneous. | B |
| LATCH | 5 | The device defaults to auto-retry (automatic) mode when encountering a thermal fault. | B |
| SNS | 6 | The sense current is not valid from the SNS pin. | B |
| ILIM | 7 | The device defaults to the internal current limit. | C |
| NC | 11 | There is no effect on the device. | D |
| VOUT | 8, 9, 10 | The current limit of the device engages. | B |
| VS | 12, 13, 14 | The device has no input supply, and therefore, does not function. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| GND | 1 | Loss of ground detection engages, and the device shuts off. | B |
| EN | 2 | The output is shutdown, and the EN pin is pulled down internally. | B |
| DIAG_EN | 3 | DIAG_EN is internally pulled down. The diagnostics are disabled. | B |
| FAULT | 4 | The fault signal is not reported. | B |
| LATCH | 13 | LATCH is internally pulled down. The device defaults to auto-retry mode when encountering a thermal fault. | B |
| SNS | 10 | The correct sense current cannot be read. | B |
| ILIM | 11 | The device defaults to the internal current limit. | C |
| NC | 11 | There is no effect on the device. | D |
| VOUT | 8, 9, 10 | There is no effect on the device. If configured, open load detection triggers. | B |
| VS | 12, 13, 14 | The device has no input supply, and therefore, does not function. | B |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| GND | 1 | EN | The channel is disabled. | B |
| EN | 2 | DIAG_EN | The EN signal effects the DIAG_EN signal and vice versa. | B |
| DIAG_EN | 3 | FAULT | Fault reporting is erroneous. The diagnostics are enabled if FAULT is pulled high. | B |
| FAULT | 4 | LATCH | Fault reporting is erroneous. The device is in auto-retry mode if FAULT is pulled high. | B |
| LATCH | 5 | SNS | The current sensing output is erroneous. The device is in auto-retry or latched off depending on the output of the SNS pin. | B |
| SNS | 6 | ILIM | The current limit and current sensing output are incorrect. | B |
| VOUT | 10 | NC | There is no effect on the device. | D |
| NC | 11 | VS | There is no effect on the device. | D |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| GND | 1 | The supply power is bypassed, and the device does not turn on. | B |
| EN | 2 | There is a potential violation of the absolute maximum rating of pin, and a possible breakdown of the ESD cell. | A |
| DIAG_EN | 3 | There is a potential violation of the absolute maximum rating of pin, and a possible breakdown of the ESD cell. | A |
| FAULT | 4 | There is a potential violation of the absolute maximum rating of pin, and a possible breakdown of the ESD cell.. | A |
| LATCH | 5 | There is a potential violation of the absolute maximum rating of pin, and a possible breakdown of the ESD cell. | A |
| SNS | 6 | There is a potential violation of the absolute maximum rating of pin, and a possible breakdown of the ESD cell. | A |
| ILIM | 7 | There is a potential violation of the absolute maximum rating of pin, and a possible breakdown of the ESD cell. | A |
| NC | 11 | There is no effect on the device. | D |
| VOUT | 8, 9, 10 | The output is pulled to the supply voltage. Short-to-battery detection is triggered if configured. | B |