SLAA991 December   2020 TMUXHS4212

 

  1.   Trademarks
  2. 1Introduction
  3. 2Major Parameters of Multiplexers
  4. 3Cascading Multiplexers Testing
  5. 4Summary

Cascading Multiplexers Testing

3.1 Simulation with S-parameters Model for Cascading Multiplexers

Now let’s look at an example of simulation with S-parameters model for two cascading TMUXHS4212 multiplexers. S-parameters are easily imported and used for circuit simulations in EDA tools like ADS. S-parameters are the shared language between simulation and measurement.
GUID-20201206-CA0I-Q3M1-NKSS-R7WPC2CRTPPW-low.png Figure 3-1 ADS Simulation of Cascading Multiplexers.
Figure 3-1 is the ADS simulation setup of two cascaded multiplexers TMUXHS4212 with S-parameter model. Figure 3-2 shows the insertion loss of the multiplexer is -1.0 db at 5 Ghz .
GUID-20201206-CA0I-CCP9-LCZN-DD2PCCKJXPFQ-low.png Figure 3-2 Insertion Loss of TMUXHS4212.

Figure 3-3 is the eye diagram of the 10-Gbps input signal, Figure 3-4 is the output eye diagram from the first multiplexer, Figure 3-5 is the output eye diagram from second multiplexer. From Figure 3-5, we can see waveform is degraded after two cascading multiplexers.

GUID-20201206-CA0I-JK6M-B0RB-VGZ8QRBJVBK0-low.png Figure 3-3 Input Signal Eye Diargam at 10Gbps.
GUID-20201206-CA0I-C0KS-CZ3Z-NT45C42RM9HT-low.png Figure 3-4 Eye Diagram after 1st Multiplexer.
GUID-20201206-CA0I-8PQ8-9JWJ-XVSZ6KFZFXJ7-low.png Figure 3-5 Eye Diagram after 2nd Multiplexer.

3.2 Testing Results with Scope

Last, let’s look at the real scope measurement and see how they correlate with the simulation result. Figure 3-6 is the waveform of the 10Gbps input signal, Figure 3-7 is the output waveform from the first multiplexer, Figure 3-8 is the output waveform form the second multiplexer. From Figure 3-7 and Figure 3-8, real measurement is correlated well with simulation result.

GUID-20201206-CA0I-3F5L-XBQR-928QTG4HTP95-low.pngFigure 3-6 Input Waveform of 10Gbps Signal.
GUID-20201206-CA0I-RBSS-DW8C-H1JZ7TVRNKQD-low.pngFigure 3-7 Output Waveform after 1st Multiplexer.
GUID-20201206-CA0I-6DJW-M8MK-DNM690VDKBJ9-low.pngFigure 3-8 Output Waveform after 2nd Multiplexer.