Click here to create a custom design using
the device with the WEBENCH® Power Designer.
Start by entering the input
voltage (VIN), output voltage (VOUT), and output current
(IOUT) requirements into WEBENCH® . For this design VIN = 12 V
(typical), VOUT = 24 V, IOUT = 500 mA
Optimize the design for key
parameters such as efficiency, footprint, and cost using the optimizer dial in
WEBENCH Power Designer.
Run electrical simulations to see
important waveforms and circuit performance (If supported by the device).
Otherwise download the spice model from website and simulate the circuit using
PSpice® for TI
Design Notes for
LM51571
When selecting the inductor (L1),
consider three key parameters: inductor current ripple ratio (RR), falling slope
of the inductor current, and Right Half Plane (RHP) zero frequency
(fRHP). RR is selected to have a balance between core loss and
copper loss. The falling slope of the inductor current must be low enough to
prevent subharmonic oscillation at high duty cycle (additional RSL resistor is
required, if not). Higher fRHP (lower inductance) allows a higher
crossover frequency and is always preferred when using a small value output
capacitor. The inductance value can be selected to set the inductor current
ripple between 30% and 70% of the average inductor current to achieve a good
compromise between RR, fRHP, and inductor falling slope
To set the output regulation
target, select the feedback resistor values as shown in the following equation:
Equation 1.
where:
VREF = 1 V
(typical)
There are a few ways to select
the proper value of the output capacitor (COUT). Select the output
capacitor value based on output voltage ripple, output overshoot, or undershoot
due to load transient. The ripple current rating of the output capacitors must
be enough to handle the output ripple current. By using multiple output
capacitors, the ripple current can be split allowing for a capacitor with a
lower ripple current to be chosen.
A Schottky diode is the preferred
type for a D1 diode due to its low forward voltage drop and small reverse
recovery charge. Low reverse-leakage current is an important parameter when
selecting the Schottky diode. The diode must be rated to handle the maximum
output voltage plus any switching node ringing. Also, it must be able to handle
the average output current.
The switching frequency of the
device can be set by a single resistor connected between RT and the GND pins
using the following equation: