SLAAE88B December 2022 – March 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
Before downloading the firmware with the GUI, prepare two files: the application firmware file and the BSL password file.
The GUI (MSPM0_BSL_GUI.exe) supports only the TI-TXT format. For details on how to generate this format image file with CCS, see 6 in Section 3.1.3.
The format of the password file is similar to the TI-TXT format as shown in Figure 3-6. The BSL password is defined in the Non-Main memory. For more information, see the technical reference manual [1][2] or the bootloader user's guide [3]. If the BSL password is not the default (all 0xFF), modify the password file. A default password file named BSL_Password32_Default.txt is available in this folder: < …\mspm0_sdk_xxxx\tools\bsl\BSL_GUI_EXE\Input >.