SLAAEC7A September   2024  – August 2025

 

  1.   1
  2. 1 Description
  3. 2 Required Peripherals
  4. 3 Design Steps
  5. 4 Design Considerations
  6. 5 Software Flow Chart
  7. 6 Application Code
  8. 7 Hardware Design
  9. 8 Results
  10. 9 Additional Resources
  11. 10Revision History
  12. 11E2E
  13. 12Trademarks

Design Considerations

  1. Number of LEDs and matrix dimensions: The matrix dimension determines the number of GPIO pins needed to run the matrix. For example, a 16 LED matrix can use 8 pins in a 4 × 4 matrix or 10 pins in a 2 × 8 matrix.
  2. LED configuration: The active states of the row and column pins is dependent on whether the matrix is in common row cathode or common row anode.
  3. Column pin values: Column pin values are set in a memory table. The exact values are determined by which pins are selected and the respective column mask. For ease of setup, selecting pins that are in numerical order with no gaps is the easiest.
  4. Column and row pin connections: When connecting pins to the LED matrix, application programming is easiest if the row pins start from the topmost row (moving down) and the column pins start from the right-most column (moving left).
  5. Timer interrupts: The speed of the interrupts affects the display period and how long each row of LEDs is on per the state machine cycle. This specific example interrupts every 5ms, preventing the human eye from noticing any flickering.
  6. Updating the memory table: The specific method of updating the memory table depends on the application. This example increments a counter (otherwise known as the display period) up to a specified value. When the counter reaches that value, the memory table is updated to set a new display.