SLAAEK3B January   2024  – August 2025 MSPM0G3507 , MSPM0H3216

 

  1.   1
  2. Description
  3. Required Peripherals
  4. Design Steps
  5. Design Considerations
  6. Software Flow Chart
    1. 5.1 Device Configuration
    2. 5.2 Required UART Packets
  7. Application Code
  8. Additional Resources
  9. E2E
  10. Revision History
  11. 10Trademarks

Design Considerations

  1. In the application code, make sure to check the SPI and UART maximum packet sizes against the requirements of the application.
  2. To increase the UART baud rate, adjust the value in the SysConfig UART tab labeled Target Baud Rate. Below this, observe the calculated baud rate change to reflect the target baud rate. This is calculated using the available clocks and dividers.
  3. Check error flags and handle them appropriately. The UART and I2C peripherals are both capable of throwing informative error interrupts. For easy debugging, this subsystem uses an enumeration and a global variable to save error codes when error codes are thrown. In real-world applications, handle errors in the code so the errors do not break the project.
  4. The current form of the project defines all of the formatted parts of the packet, such as UART_START_BYTE, UART_READ_SPI_BYTE, and UART_WRITE_SPI_BYTE. These are accompanied by definitions to specify where in the packet header these commands are found. Values in the implementation can be changed. Make sure that the UART start and read or write bytes are bytes that are not expected in the application.