SLAAEK3B January   2024  – August 2025 MSPM0G3507 , MSPM0H3216

 

  1.   1
  2. Description
  3. Required Peripherals
  4. Design Steps
  5. Design Considerations
  6. Software Flow Chart
    1. 5.1 Device Configuration
    2. 5.2 Required UART Packets
  7. Application Code
  8. Additional Resources
  9. E2E
  10. Revision History
  11. 10Trademarks

Application Code

Some users want to change the specific values that are used by the UART packet header, or the maximum packet size. This change is done by modifying the #define values found in the beginning of the uart_to_spi_bridge.c file, as shown in the following code.

/* Define UART Header and Start Byte*/
#define UART_HEADER_LENGTH  0x02
#define UART_START_BYTE     0xF8
#define UART_READ_SPI_BYTE  0xFA
#define UART_WRITE_SPI_BYTE 0xFB
#define RW_INDEX            0x00
#define LENGTH_INDEX        0x01

/*Define max packet sizes*/
#define SPI_MAX_PACKET_SIZE     (16)
#define UART_MAX_PACKET_SIZE    (SPI_MAX_PACKET_SIZE + UART_HEADER_LENGTH)

Many portions of the code are intended to be used for error detection and handling. At these points in the code, the user can use additional error handling or reporting for a more robust application. For example, the following code segment demonstrates a way to check for errors in SPI transmissions, and sets an error flag in the event of an error. The user can quit sending and change the UART Bridge Status here to reflect the error. This and many other areas in the code have options for error consideration.

for(int i = 0; i < gMsgLength; i++){
                if(!DL_SPI_transmitDataCheck8(SPI_0_INST, gSPIData[i])){
                    gError = ERROR_SPI_WRITE_FAILED;
        }
}