SLAAEK6 June 2024 ULC1001 , ULC1001-Q1
The mechanical design procedure involves designing each individual component and assembling the components to build the LCS. In particular, the design procedure (Figure 3-3 and Figure 3-4) can be described by the following steps :
Figure 3-3 Mechanical Design Procedure of Flat Lens LCS: Lens + Glue + Transducer + Thin Film = Lens Cover
In LCS design, the most critical is to design a Lens Cover where the lens and the transducer is well matched. TI uses a FEA simulation tool- COMSOL Multiphysics to simulate the interactions between the components. Other FEA simulation tools such as Ansys can be used as well.
The goal of the simulation is to obtain the highest lens surface acceleration by sweeping the dimensional parameters of the lens and piezo transducer.