SLAAEP3 December   2025 ULC1001

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Acronyms
  5. 2 Introduction
  6. 3 Impedance Response
    1. 3.1 Piezo Only
    2. 3.2 Lens Cover
    3. 3.3 Lens Cover System (LCS)
  7. 4 Equivalent Circuit Model of LCS
  8. 5 LC Filter for LCS
  9. 6 Water Cleaning
  10. 7 Power Consumption
  11. 8 Reliability
  12. 9 Other Tests
    1. 9.1 De-ice
    2. 9.2 Mud Cleaning
    3. 9.3 Optical Interference
    4. 9.4 Waterproof Capability
  13. 10Resources

Water Cleaning

Figure 6-1 shows the GUI setting (GUI version: ULC1001 2.4.10) for the LCS. For more info about the ULC1001 GUI, please refer to the tutorial video on ti.com.

 GUI Setting: Calibrated ResultFigure 6-1 GUI Setting: Calibrated Result

Figure 6-2 shows the GUI settings for water mode.

 GUI Setting: Water Mode for CleaningFigure 6-2 GUI Setting: Water Mode for Cleaning

Figure 6-3 illustrates the water cleaning performance observed in the water mode operation. It is evident that the majority of water droplets have been expelled; however, fine mist remain along the edge of the lens (dissipate quickly in typical applications). This phenomenon is typical, as the acceleration is maximized at the center of the lens and diminishes to zero at the outer edges.

 Water Cleaning Result: Before Cleaning versus After CleaningFigure 6-3 Water Cleaning Result: Before Cleaning versus After Cleaning