SLAAEU1 August 2025 MSPM0L1306 , MSPM0L1306
A resistive touch screen works by applying a voltage across a resistor network and measuring the change in resistance at a given point on the matrix where a screen is touched by an input stylus, pen, or finger. This consists of two transparent resistive layers made by ITO. The change in the resistance ratio marks the location on the touch screen. The two most popular resistive architectures use 4-wire or 5-wire configurations. The related software can be accessed at MSPM0L1306-RESISTIVE-TOUCH-APPSW.