SLAAEU9 June 2026 TAS5805M , TAS5825M , TAS5827 , TAS5828M
To prevent signal distortion after Class-D amplification, it is essential to first determine the maximum voltage that the Class-D amplifier can output. The TAS58xx utilizes BD/1SPW/Hybrid mode modulation to generate a high-frequency PWM wave in the full-bridge circuit, which is then filtered by the subsequent magnetic beads or LC filter to obtain an amplified high-fidelity analog audio signal. Theoretically, a larger input signal leads to a higher PWM duty cycle in the subsequent power stage, resulting in a higher output voltage; when the modulated PWM reaches a 100% duty cycle, the subsequent speaker receives the maximum non-clipped voltage. For instance, when PVDD = 12V, the maximum non-clipping sinusoidal voltage peak that the subsequent stage can obtain is ±12V. However, in practical circuits, the internal resistance of the MOSFETs and inductors creates a voltage drop, so the maximum voltage actually achieved by the speaker will be slightly lower than PVDD.
The simplified Class-D circuit is shown in Figure 1-1 below. Taking into account the voltage division effect of the MOSFET and inductor internal resistance, the maximum voltage that the load can actually receive is:
Figure 1-1 Class D Equivalent Circuit