SLAU573C November 2015 – October 2019
For most MSP430 devices, there are two ways to invoke the BSL: by the application software or by applying a hardware entry sequence.
The MSP-BSL can apply the entry sequence (see Figure 3) to the target. This entry sequence can be used for devices with shared or dedicated JTAG pins. The entry sequence can be triggered by setting the communication speed of the MSP-BSL to 9601 baud (for UART) or to the baud rate of any mode with a BSL entry sequence; for example, 100001 baud for I2C mode with BSL entry sequence (see Table 1).
Figure 3. BSL Entry Sequence With Shared and Dedicated JTAG Pins NOTE
For further information on the entry sequence, see the user's guides listed in Section 1.1.