SLAU923B June 2025 – April 2026 MSPM0H3215 , MSPM0H3216 , MSPM0H3216-Q1
The low-frequency subsystem (LFSS) contains an independent watchdog timer (IWDT).
The independent watchdog timer (IWDT) is a device-independent supervisor which monitors code execution and overall hang up scenarios of the device. If the application software does not successfully reset the watchdog within the programmed time, the watchdog generates a POR reset to the device.
For more information on the LFSS independent watchdog timer, see the IWDT chapter.