SLCS141M May 2003 – December 2024 LM2903-Q1 , LM2903B-Q1
PRODUCTION DATA
Output current is determined by the load/pull-up resistance and logic/pull-up voltage. The output current produces a output low voltage (VOL) from the comparator. In which VOL is proportional to the output current. Use Figure 2-21 to determine VOL based on the output current.
The output current can also effect the transient response. More explanation is in the next section.