SLDA058 March 2021 TUSS4470
Because the TDC1000's architecture is optimized for higher frequency liquid-coupled applications, utilizing the TDC1000 for air-coupled evaluation requires more fine tuning and patience than the TUSS4470. Table 2-4 provides recommended values as a starting point, allowing a ToF in the range 128 ✕ T0 up to 128 ✕ T0 + 1024 ✕ T0. Values are given in the GUI format, see the TDC1000-C2000EVM GUI and the TDC1000 data sheet programming section for corresponding register values. For a short ToF measurement time line graphic and T0, T1 definitions, see Appendix B.
| GUI Setting | GUI Value | Comments |
|---|---|---|
| TOF_MEAS_MODE | 0 | Measurement mode 0 for mono-static ToF measurements |
| Recieve Mode | Single or Multi- Echo | |
| CLOCKIN_DIV | Div by 1 | Set T0 with CLOCKIN_DIV |
| FORCE_SHORT_TOF | Enabled | The short ToF mode allows the common-mode voltage settling time (128 ✕ T0) to occur before the TX burst, so that the COMPIN signal will be less noisy and the listen period may be maximized. |
|
TOF_TIMEOUT_CTRL |
1024 ✕ T0 | This allows a maximum echo listen period of approximately 4.6 ms. |
| NUM_TX | 10 - 15 pulses | This is a good starting point for producing a strong return echo. |
| NUM_RX | No RX Event Count | This allows STOP signals to be generated for the duration of TOF_TIMEOUT_CTRL, avoiding ending the measurement due to an erroneously generated STOP. |
| PGA_GAIN | 21 dB | The maximum gain is recommended for air-coupled evaluation. |
| ECHO_QUAL_THLD | -35 mV | The most sensitive echo threshold setting may be necessary to trigger a STOP. |
| LNA_FB | Resistive | Required for transducers in this frequency range. |
| AUTOZERO_PERIOD | 64 ✕ To | In short ToF mode, this period occurs before the TX burst and can be adjusted if needed. |
| SHRT_TOF_BLNK_PRD | 128 ✕ T0 | This should allow plenty of time for noise coupled from the TX line to settle and have a clean COMPIN for viewing the return echo. |
Evaluation Notes:
Signals of interest: START, STOP, COMPIN, TX.
For short range measurements, the blanking period may need to be shortened so the return echo can trigger a STOP. Depending on the transducer frequency, the transducer ringing decay could couple noise onto the COMPIN signal path causing a false STOP to be triggered at the beginning of the listen period. If this occurs, the blanking period can be set to mask this noise, or other means of ignoring a false STOP may be required at the designer's discretion. This is a good reason to set an unlimited NUM_RX event count for initial evaluation.