SLLA486B
May 2020 – October 2024
ISO1042
,
ISO1042-Q1
,
ISO1044
,
ISO1050
,
ISOW1044
1
Top Design Questions About Isolated CAN Bus Design
Trademarks
1
When Do I Need to Isolate CAN?
2
What are the Options Available to Isolate CAN Bus?
3
Now That I Have Isolated CAN Signal Path, How Do I Generate Isolated Power?
4
What’s the Reason Behind Terminating the Bus, Do I Need it, and How to Achieve it?
5
What’s the Difference Between Common Mode Range and Bus Standoff Mentioned in Data Sheet?
6
Now That I Have Taken Care of the Termination Resistor, What Other Components do I Need on the Bus Side?
7
When Connecting Isolated CAN Nodes in a Network, What Should be Done with the Floating Bus-Side Ground Connection?
8
Is There a Limitation on Minimum Data Rate That I Can Operate? What About the Maximum Data Rate Achievable in a Network?
9
Is There a Limit on Maximum Number of Nodes That I Can Connect in CAN Network?
10
What Factors Decide the Maximum Communication Distance in a CAN Network?
11
What is the Maximum Value of Bus Capacitance That Can be Introduced Between CANH to GND and CANL to GND? Can Higher Capacitance Damage the Device?
12
Is There a Way to Extend the Maximum Communication Distance?
13
What is Stub Length? What are the Design Considerations Around it?
14
I am Seeing Larger Differential CAN Voltage for Some Bits of CAN Packet Compared to Rest of the Packet When I am Communicating in a Network with Multiple Nodes Connected. Why?
15
References
16
Revision History
15
References
Texas Instruments,
ISO1044 data sheet
Texas Instruments,
Controller Area Network Physical Layer Requirements