SLLA486B May 2020 – October 2024 ISO1042 , ISO1042-Q1 , ISO1044 , ISO1050 , ISOW1044
Each node presents a certain differential load across the CAN bus which is specified as RID (differential input resistance) in the Receiver Electrical Characteristics section of the device data sheet. For ISO1044 and ISOW1044 is specified at minimum of 40 kohm. Other than the two 120 ohm termination resistors on far ends of the network, each node’s differential resistance combines in parallel to load the transmitter that is about to drive dominant on the bus. The equivalent parallel resistance that a driver should see needs to be more than 45 ohm because 45 ohm is the minimum load a driver is specified to drive and produce a minimum differential voltage of 1.4 V (as specified in Driver Electrical Characteristics). So in the case of ISO1044 and ISOW1044, if we connect 222 nodes on the bus, the equivalent differential resistance all CAN nodes offer on the bus is 40000/222 = 180 ohm. This 180 ohm in parallel to two 120 ohm termination resistors gives a 45 ohm equivalent loading on the driver. This is the theoretical limit on the maximum number of nodes on a CAN bus. Practical system aspects will limit this further.