SLLA486C May   2020  – May 2026 ISO1042 , ISO1042-Q1 , ISO1044 , ISO1050 , ISOW1044 , ISOW1050

 

  1.   1
  2.   Top Design Questions About Isolated CAN Bus Design
  3.   Trademarks
  4. 1 When Do I Need to Isolate CAN?
  5. 2 What are the Options Available to Isolate CAN Bus?
  6. 3 Now That I Have Isolated CAN Signal Path, How Do I Generate Isolated Power?
  7. 4 What’s the Reason Behind Terminating the Bus, Do I Need it, and How to Achieve it?
  8. 5 What’s the Difference Between Common Mode Range and Bus Standoff Mentioned in Data Sheet?
  9. 6 Now That I Have Taken Care of the Termination Resistor, What Other Components do I Need on the Bus Side?
  10. 7 When Connecting Isolated CAN Nodes in a Network, What Should be Done with the Floating Bus-Side Ground Connection?
  11. 8 Is There a Limitation on Minimum Data Rate That I Can Operate? What About the Maximum Data Rate Achievable in a Network?
  12. 9 Is There a Limit on Maximum Number of Nodes That I Can Connect in CAN Network?
  13. 10What Factors Decide the Maximum Communication Distance in a CAN Network?
  14. 11What is the Maximum Value of Bus Capacitance That Can be Introduced Between CANH to GND and CANL to GND? Can Higher Capacitance Damage the Device?
  15. 12Is There a Way to Extend the Maximum Communication Distance?
  16. 13What is Stub Length? What are the Design Considerations Around it?
  17. 14I am Seeing Larger Differential CAN Voltage for Some Bits of CAN Packet Compared to Rest of the Packet When I am Communicating in a Network with Multiple Nodes Connected. Why?
  18. 15References
  19. 16Revision History

Now That I Have Isolated CAN Signal Path, How Do I Generate Isolated Power?

Multiple options are available for isolated power generation for a CAN node. If the field side (for example, bus side) circuitry needs more power than just powering the CAN transceiver, push-pull transformer drivers like TI’s SN6505B driving an external transformer is a simple-to-use and low cost solution as shown in Figure 3-1. For space-constrained applications the ISOW1044 provides signal isolation, DC/DC converter, and a CAN FD transceiver in a single chip to reduce solution size and simplify the design process, as shown in Figure 3-2. Sometimes in certain industrial applications, such as DeviceNet, a 24-V supply is available on the field side which can be used as shown in Figure 3-4. To learn more on this topic, read the application brief, How to Isolate Signal and Power in Isolated CAN Systems. Device Update: ISOW1050 is the latest release for Isolated CAN with Integrated Power for Cost optimized systems to achieve best EMC performance. To improve your design using ISOW1050 see Enhance Design Performance using Integrated Power and Digital Isolation Design. To achieve best EMC performance with ISOW1050, see Achieving Best EMC Performance for Signal Isolators with Integrated Power

 Isolated Power Generation Using Push-Pull
                    TopologyFigure 3-1 Isolated Power Generation Using Push-Pull Topology
 Isolated Signal and Power Using Small
                    Form-Factor ISOW1044Figure 3-2 Isolated Signal and Power Using Small Form-Factor ISOW1044
 Isolated Signal and Power
                    Using ISOW1050 for Best EMC Figure 3-3 Isolated Signal and Power Using ISOW1050 for Best EMC
 DeviceNet Application SchematicFigure 3-4 DeviceNet Application Schematic