SLLA590 May   2022 THVD8000 , THVD8010

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2THVD80x0 Devices Theory of Operation and Limitations of Use
    1. 2.1 Overview and Similarities between Standard RS-485 Transceivers and THVD80xo Devices
    2. 2.2 Differences between Standard RS-485 Transceivers and THVD8000/8010
    3. 2.3 Standard Approach to Using THVD80xo Devices to Communicate over Power Lines
    4. 2.4 Drawbacks to Standard Approach with Higher Voltage Systems
  5. 3Integration of Line Driver with THVD80x0 Devices to Drive Low Impedance Loads
    1. 3.1 Overcoming Drive Strength Requirement with A Line Driver Amplifier
    2. 3.2 Modification to Typical System Signal Chain Path Through Integration of Line Driver
  6. 4High Voltage Interface and Communication Interface Power Supply
    1. 4.1 Line Driver Output and Input RX signal Protection Circuit
    2. 4.2 High-Voltage Interface
    3. 4.3 Receive Path Optional Bandpass
  7. 5System Level View and Relation to Higher Voltage Implementations
    1. 5.1 Powering the Powerline Communication System
    2. 5.2 System Overview with Selected Test Results
    3. 5.3 Changes to Design for Higher Voltage AC or DC Applications
  8. 6Summary
  9. 7References

High-Voltage Interface

The next piece of the system is one of the simplest, yet one of the most important aspects of the system, that is the high voltage interface. For AC applications this interface is shown in Figure 4-2 and it is simply a transformer and high voltage capacitor.

Figure 4-2 HV Interface for High Voltage/Low Impedance AC Power Lines

This circuit serves one main purpose – to act as a bandpass filter to allow the communication signal to be coupled onto the main line while preventing the low frequency AC signal from feeding back into the protection circuit. This becomes clearer when the equivalent transformer circuit is used. This is shown in Figure 4-3.

Figure 4-3 HV Interface Equivalent Circuit

The capacitor and transformer together create a bandpass filter. The goal of this filter is to filter out the AC mains frequency (~60Hz) while keeping the communication modulation frequency within the pass band. The parameters of the transformer can be found in the transformers datasheet where leakage inductance is L_leak_p + L_leak_s’, core resistance is Rc (if not shown assume RC to be open circuit), core inductance is Lm, the primary winding resistance is Rs_p, and the secondary winding is Rs_s. Please note that the above figure has “transformed” the equivalent circuit to remove the turns ratio – to convert secondary components to their “transformed” version, s, so that an accurate model is retained, divide the original impedance value by the turn’s ratio (Primary to Secondary) squared. For most transformer datasheets the only value you may have to transform is Rs_s which would be Rs_s’ = Rs_s/ (turn’s ratio) ^2.

After the bandwidth has been sorted out the capacitor must be rated for high voltage applications as it will take the brunt of the incoming signal. For a 110 VAC too 220 VAC application a 1.5 kV rated capacitor was used.

If the end power line is not AC and is high voltage DC – the transformer is unnecessary and only the high voltage capacitor is needed as the capacitor will block the high DC voltage.