SLLSFT3B November 2025 – November 2026 MC121-Q1
PRODUCTION DATA
The MC121-Q1 provides three PWM modulation modes: synchronous, asynchronous and hybrid. The PWM_MODE bits sets hybrid, synchronous, or asynchronous modulation for motor current during PWM OFF time and θDEMAG time, as described in Section 6.3.1.7. Figure 6-16, Figure 6-17, and Figure 6-18 show timing diagrams for asynchronous, synchronous, and hybrid recirculation states during θDEMAG respectively.
During synchronous mode, both low-side FETs turn on during the PWM OFF time. Synchronous mode reduces power loss by conducting the free-wheeling current through the FET instead of the body diode. However, depending on turn-off current and motor winding inductance, there can be reverse current conduction during synchronous modulation resulting in negative torque and lower motor speed.
During asynchronous mode, only one low-side FET remains on during the PWM OFF time while all other FETs are disabled and the freewheeling current is conducted through the body diode of the other low-side FET. In asynchronous mode, there is no reverse-current flow during PWM off time but the power loss can be higher due to body diode conduction.
The MC121-Q1 features a hybrid modulation scheme which combines both modes to reduce power loss during free-wheeling while preventing reverse-current flow.
Table 6-1 shows the H-bridge states for the output PWM. H indicates HS FET in given OUTx leg is ON, L indicates LS FET in given OUTx leg is ON, Z indicates both FETs in given OUTx legs are in Hi-Z. The hall offset signal is the internal signal determined from the Hall sensor state and device settings. The hall offset signal determines the output switching states in the commutation algorithm state machine. The input PWM duty cycle and commutation mode (square/soft) determine the instantaneous output PWM duty cycle, DOUT.
| Driver State | Description |
Modulation mode set by PWM_MODE |
Hall Offset Signal | OUT1 | OUT2 |
|---|---|---|---|---|---|
| DOUT | PWM ON time/duty cycle | X | L | L | H |
| X | H | H | L | ||
| (1-DOUT), Current Limiting, θDEMAG | Motor current recirculation during PWM OFF time/duty or during current limiting off time, or phase demagnetization time before a commutation event | Asynchronous mode | L | L | Z |
| H | Z | L | |||
| Synchronous mode | X | L | L |
Figure 6-19 shows the motor current flow through the H-bridge during PWM ON time, PWM OFF time, and demagnetization states. Refer to Section 6.3.1.6.3 for more details on demagnetization state.
The hybrid PWM mode enables both low-side FETs during the PWM OFF time (same as synchronous mode) to avoid recirculating the motor current through the body diode. A, zero-current detector disables the applicable low-side FET to place the H-bridge in the asynchronous mode to prevent reverse-current flow. By automatically switching between synchronous and asynchronous modes during each PWM cycle, the MC121-Q1 reduces device power loss while avoiding back EMF generating unintended negative current in the motor winding.
Table 6-2 shows the settings for the PWM_MODE bits to configure the PWM modulation mode.
| PWM_MODE Bits | PWM and Current Limiting OFF Time | Demagnetization State |
|---|---|---|
| 000b | Hybrid | Hybrid |
| 001b | Hybrid | Asynchronous |
| 010b | Asynchronous | Hybrid |
| 011b | Synchronous | Hybrid |
| 100b | Synchronous | Synchronous |
| 101b | Synchronous | Asynchronous |
| 110b | Asynchronous | Synchronous |
| 111b | Asynchronous | Asynchronous |