SLLSFX3B October 2024 – June 2026 TCAN844-Q1
PRODUCTION DATA
The TCAN844(V)-Q1 is designed to be a passive or no load to the CAN bus if the device is unpowered. The bus pins were designed to have low leakage currents when the device is unpowered, so the device does not load the bus. This is critical if some nodes of the network are unpowered while the rest of the of network remains operational.
The logic pins also have low leakage currents when the device is unpowered, so the pins do not load other circuits which may remain powered.